Other Parts Discussed in Thread: CC3200
想請問有人知道SimpleLinkGeneralEventHandler [GENERAL EVENT] - ID=[2] Sender=[0]的意思嗎?
因為目前CC3200每次重新開機都會出現此錯誤,想要知道是甚麼原因造成
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: CC3200
想請問有人知道SimpleLinkGeneralEventHandler [GENERAL EVENT] - ID=[2] Sender=[0]的意思嗎?
因為目前CC3200每次重新開機都會出現此錯誤,想要知道是甚麼原因造成
建议升级到最新的SDK和service pack进行测试。报错原因可在device.h找到,具体如下:
/* Errors returned from the general error async event */
/*****************************************************************************/
/* Send types */
typedef enum
{
SL_ERR_SENDER_HEALTH_MON,
SL_ERR_SENDER_CLI_UART,
SL_ERR_SENDER_SUPPLICANT,
SL_ERR_SENDER_NETWORK_STACK,
SL_ERR_SENDER_WLAN_DRV_IF,
SL_ERR_SENDER_WILINK,
SL_ERR_SENDER_INIT_APP,
SL_ERR_SENDER_NETX,
SL_ERR_SENDER_HOST_APD,
SL_ERR_SENDER_MDNS,
SL_ERR_SENDER_HTTP_SERVER,
SL_ERR_SENDER_DHCP_SERVER,
SL_ERR_SENDER_DHCP_CLIENT,
SL_ERR_DISPATCHER,
SL_ERR_NUM_SENDER_LAST=0xFF
}SlErrorSender_e;
typedef enum
{
SL_DRIVER_API_DEVICE_SL_START = 0,
SL_DRIVER_API_DEVICE_SL_STOP,
SL_DRIVER_API_NETAPP_PING_START,
SL_DRIVER_API_SOCKET_CONNECT,
SL_DRIVER_API_SOCKET_ACCEPT,
SL_DRIVER_API_SOCKET_SELECT,
SL_DRIVER_API_SOCKET_RECV,
SL_DRIVER_API_SOCKET_RECVFROM
} SlDriverAPIWithTimeout_e;
/* Error codes */
#define SL_ERROR_STATIC_ADDR_SUBNET_ERROR (-60) /* network stack error*/
#define SL_ERROR_ILLEGAL_CHANNEL (-61) /* supplicant error */
#define SL_ERROR_SUPPLICANT_ERROR (-72) /* init error code */
#define SL_ERROR_HOSTAPD_INIT_FAIL (-73) /* init error code */
#define SL_ERROR_HOSTAPD_INIT_IF_FAIL (-74) /* init error code */
#define SL_ERROR_WLAN_DRV_INIT_FAIL (-75) /* init error code */
#define SL_ERROR_WLAN_DRV_START_FAIL (-76) /* wlan start error */
#define SL_ERROR_FS_FILE_TABLE_LOAD_FAILED (-77) /* init file system failed */
#define SL_ERROR_PREFERRED_NETWORKS_FILE_LOAD_FAILED (-78) /* init file system failed */
#define SL_ERROR_HOSTAPD_BSSID_VALIDATION_ERROR (-79) /* Ap configurations BSSID error */
#define SL_ERROR_HOSTAPD_FAILED_TO_SETUP_INTERFACE (-80) /* Ap configurations interface error */
#define SL_ERROR_MDNS_ENABLE_FAIL (-81) /* mDNS enable failed */
#define SL_ERROR_HTTP_SERVER_ENABLE_FAILED (-82) /* HTTP server enable failed */
#define SL_ERROR_DHCP_SERVER_ENABLE_FAILED (-83) /* DHCP server enable failed */
#define SL_ERROR_PREFERRED_NETWORK_LIST_FULL (-93) /* supplicant error */
#define SL_ERROR_PREFERRED_NETWORKS_FILE_WRITE_FAILED (-94) /* supplicant error */
#define SL_ERROR_DHCP_CLIENT_RENEW_FAILED (-100) /* DHCP client error */
/* WLAN Connection management status */
#define SL_GENERAL_ERROR_CON_MGMT_STATUS_UNSPECIFIED (-102)
#define SL_GENERAL_ERROR_CON_MGMT_STATUS_AUTH_REJECT (-103)
#define SL_GENERAL_ERROR_CON_MGMT_STATUS_ASSOC_REJECT (-104)
#define SL_GENERAL_ERROR_CON_MGMT_STATUS_SECURITY_FAILURE (-105)
#define SL_GENERAL_ERROR_CON_MGMT_STATUS_AP_DEAUTHENTICATE (-106)
#define SL_GENERAL_ERROR_CON_MGMT_STATUS_AP_DISASSOCIATE (-107)
#define SL_GENERAL_ERROR_CON_MGMT_STATUS_ROAMING_TRIGGER (-108)
#define SL_GENERAL_ERROR_CON_MGMT_STATUS_DISCONNECT_DURING_CONNECT (-109)
#define SL_GENERAL_ERROR_CON_MGMT_STATUS_SG_RESELECT (-110)
#define SL_GENERAL_ERROR_CON_MGMT_STATUS_ROC_FAILURE (-111)
#define SL_GENERAL_ERROR_CON_MGMT_STATUS_MIC_FAILURE (-112)
/* end of WLAN connection management error statuses */
#define SL_ERROR_WAKELOCK_ERROR_PREFIX (-115) /* Wake lock expired */
#define SL_ERROR_LENGTH_ERROR_PREFIX (-116) /* Uart header length error */
#define SL_ERROR_MDNS_CREATE_FAIL (-121) /* mDNS create failed */
#define SL_ERROR_GENERAL_ERROR (-127)
#define SL_DEVICE_GENERAL_CONFIGURATION (1)
#define SL_DEVICE_GENERAL_CONFIGURATION_DATE_TIME (11)
#define SL_DEVICE_GENERAL_VERSION (12)
#define SL_DEVICE_STATUS (2)
看起來只要再call sl_Start();就會再出現這個事件,有甚麼辦法可以消除這事件嗎?
可以清除NWP的register嗎?