This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3200: SimpleLinkGeneralEventHandler [GENERAL EVENT] - ID=[2] Sender=[0]

Other Parts Discussed in Thread: CC3200

想請問有人知道SimpleLinkGeneralEventHandler [GENERAL EVENT] - ID=[2] Sender=[0]的意思嗎?

因為目前CC3200每次重新開機都會出現此錯誤,想要知道是甚麼原因造成

  • 请问SDK和service pack版本分别是什么?
  • SDK1.3.0 and servicepack_1.0.1.13-2.11.0.1.bin
  • 建议升级到最新的SDK和service pack进行测试。报错原因可在device.h找到,具体如下:

    /* Errors returned from the general error async event                        */
    /*****************************************************************************/
    
    /* Send types */
    typedef enum
    {
        SL_ERR_SENDER_HEALTH_MON,
        SL_ERR_SENDER_CLI_UART,
        SL_ERR_SENDER_SUPPLICANT,
        SL_ERR_SENDER_NETWORK_STACK,
        SL_ERR_SENDER_WLAN_DRV_IF,
        SL_ERR_SENDER_WILINK,
        SL_ERR_SENDER_INIT_APP,
        SL_ERR_SENDER_NETX,
        SL_ERR_SENDER_HOST_APD,
        SL_ERR_SENDER_MDNS,
        SL_ERR_SENDER_HTTP_SERVER,
        SL_ERR_SENDER_DHCP_SERVER,
        SL_ERR_SENDER_DHCP_CLIENT,
        SL_ERR_DISPATCHER,
        SL_ERR_NUM_SENDER_LAST=0xFF
    }SlErrorSender_e; 
    
    
    typedef enum
    {
        SL_DRIVER_API_DEVICE_SL_START = 0,
        SL_DRIVER_API_DEVICE_SL_STOP,
        SL_DRIVER_API_NETAPP_PING_START,
        SL_DRIVER_API_SOCKET_CONNECT,
        SL_DRIVER_API_SOCKET_ACCEPT,
        SL_DRIVER_API_SOCKET_SELECT,
        SL_DRIVER_API_SOCKET_RECV,
        SL_DRIVER_API_SOCKET_RECVFROM
       
    } SlDriverAPIWithTimeout_e;
    
    
    /* Error codes */
    #define SL_ERROR_STATIC_ADDR_SUBNET_ERROR                   (-60)  /* network stack error*/
    #define SL_ERROR_ILLEGAL_CHANNEL                            (-61)  /* supplicant error */
    #define SL_ERROR_SUPPLICANT_ERROR                           (-72)  /* init error code */
    #define SL_ERROR_HOSTAPD_INIT_FAIL                          (-73)  /* init error code */
    #define SL_ERROR_HOSTAPD_INIT_IF_FAIL                       (-74)  /* init error code */
    #define SL_ERROR_WLAN_DRV_INIT_FAIL                         (-75)  /* init error code */
    #define SL_ERROR_WLAN_DRV_START_FAIL                        (-76)  /* wlan start error */
    #define SL_ERROR_FS_FILE_TABLE_LOAD_FAILED                  (-77)  /* init file system failed */
    #define SL_ERROR_PREFERRED_NETWORKS_FILE_LOAD_FAILED        (-78)  /* init file system failed */
    #define SL_ERROR_HOSTAPD_BSSID_VALIDATION_ERROR             (-79)  /* Ap configurations BSSID error */
    #define SL_ERROR_HOSTAPD_FAILED_TO_SETUP_INTERFACE          (-80)  /* Ap configurations interface error */
    #define SL_ERROR_MDNS_ENABLE_FAIL                           (-81)  /* mDNS enable failed                */
    #define SL_ERROR_HTTP_SERVER_ENABLE_FAILED                  (-82)  /* HTTP server enable failed         */
    #define SL_ERROR_DHCP_SERVER_ENABLE_FAILED                  (-83)  /* DHCP server enable failed         */
    #define SL_ERROR_PREFERRED_NETWORK_LIST_FULL                (-93)  /* supplicant error  */
    #define SL_ERROR_PREFERRED_NETWORKS_FILE_WRITE_FAILED       (-94)  /* supplicant error  */
    #define SL_ERROR_DHCP_CLIENT_RENEW_FAILED                   (-100) /* DHCP client error */
    /* WLAN Connection management status */
    #define SL_GENERAL_ERROR_CON_MGMT_STATUS_UNSPECIFIED                (-102)  
    #define SL_GENERAL_ERROR_CON_MGMT_STATUS_AUTH_REJECT                (-103)  
    #define SL_GENERAL_ERROR_CON_MGMT_STATUS_ASSOC_REJECT               (-104)  
    #define SL_GENERAL_ERROR_CON_MGMT_STATUS_SECURITY_FAILURE           (-105)  
    #define SL_GENERAL_ERROR_CON_MGMT_STATUS_AP_DEAUTHENTICATE          (-106)  
    #define SL_GENERAL_ERROR_CON_MGMT_STATUS_AP_DISASSOCIATE            (-107)  
    #define SL_GENERAL_ERROR_CON_MGMT_STATUS_ROAMING_TRIGGER            (-108)  
    #define SL_GENERAL_ERROR_CON_MGMT_STATUS_DISCONNECT_DURING_CONNECT  (-109)  
    #define SL_GENERAL_ERROR_CON_MGMT_STATUS_SG_RESELECT                (-110)  
    #define SL_GENERAL_ERROR_CON_MGMT_STATUS_ROC_FAILURE                (-111)  
    #define SL_GENERAL_ERROR_CON_MGMT_STATUS_MIC_FAILURE                (-112)  
    /* end of WLAN connection management error statuses */
    #define SL_ERROR_WAKELOCK_ERROR_PREFIX                      (-115)  /* Wake lock expired */
    #define SL_ERROR_LENGTH_ERROR_PREFIX                        (-116)  /* Uart header length error */
    #define SL_ERROR_MDNS_CREATE_FAIL                           (-121)  /* mDNS create failed */
    #define SL_ERROR_GENERAL_ERROR                              (-127)
    
    
    
    #define SL_DEVICE_GENERAL_CONFIGURATION           (1)
    #define SL_DEVICE_GENERAL_CONFIGURATION_DATE_TIME (11)
    #define SL_DEVICE_GENERAL_VERSION                 (12)
    #define SL_DEVICE_STATUS                          (2)
    

  • 升級可以解決這問題嗎?因為目前產品已經出廠了...

    找得到Sender==>SL_ERR_SENDER_HEALTH_MON,可是不知道是甚麼意思?前面ID[2]找不到....


    想請問遇到這事件,可以做些甚麼??
  • 看起來只要再call sl_Start();就會再出現這個事件,有甚麼辦法可以消除這事件嗎?

    可以清除NWP的register嗎?

  • 如果在你们的板子上运行SDK里面的例程会有这个问题吗?启动的时候调用了哪些API?
  • 使用SDK的也會有這問題,一使用sl_Start();就會出現這事件....然後就不動了

    事件發生後使用sl_Stop()跟Hibernate重啟後,程式一樣遇到sl_Start() API就會出現此事件...

    可以消除NWP的這個旗標?或者?