Other Parts Discussed in Thread: UNIFLASH,
自己设计CC3120PCB板,现在用串口UNIFLASH下载服务包到Sflash,提示:operation failed:slimagecreator.exe:bootloadererror,timeout reading data
电路如下:
1.电源3.3V供电正常
2.pin32 nRESET引脚 100K//0.1uf阻容复位
3.pin2 nHIB引脚 100K上拉到VCC
4,pin51,pin52 RTC晶振外接一个32.768KHz无源晶振(CC3120内部是否有32.768KHz晶振,不需要这个外接晶振?)
pin22,pin23 外接WLAN无源晶振40MHz(CC3120内部是否有40MHz晶振,不需要这个外接晶振?)
5. pin21 sop2 2.7K电阻下拉到GND
pin34 sop1 1K电阻上拉到VCC
pin35 sop0 100K下拉到GND
6. pin11、12、13、14外接16Mbit falsh
7. pin61 UART1_nCTS引脚无上拉、下拉电阻
pin50 UART1_nRTS 引脚100K电阻下拉到GND
pin55 UART1_TX 引脚100K电阻上拉到GND
pin57 UART1_RX 引脚100K电阻上拉到GND
现在用USB转串口工具,2线制连接pin55 pin57两个引脚(不存在TX,RX接反的情况,因为互换测试过,也没成功) ,用的115200bps速率(CC3120对速率是否有要求 ), 用UNIFLAH下载服务包到pin11、12、13、14外接16Mbit falsh ,出现提示超时CC,怎么回事呢?