This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

cc3000怎么使用



TI技术专家好。请教几个问题;

1  我看大家在这里讨论关于比如MSP430和cc3000的相关实验,我没搞明白,他们现在就用芯片做的板子呢还是在TI买的板子,然后就可以试着调试sdk的代码了吗,还是怎么回事?

2 如果是从TI拿到样片做出板子来调试的话,整个的板子的结构是什么样的呢?  TI网站上已经有了cc3000的连接图示,是不是就是拿MSP430的spi脚直接分别对应连上cc3000的spi对应管脚就ok了吗,还是怎么连接 ?

3 我下载MSP430的工具,填写好相关项后,点击submit,然后出现的页面是“这个页面打不开了”,或者“你访问的网页已经不存在了”。这个是真的打不开了,还是后台实际上已经提交ok了 ?

4 如果3中描述的确实是网络问题,或者网页问题,烦请提供一份关于MSP430的sdk包给我一下。我的邮箱是  dushipingjlu@gmail.com

我是刚刚接触CC3000,很多不明白,我的问题太弱了,烦请指导下。谢谢。

  • Shiping,

    您好!请参考我的回复如下:

    1  我看大家在这里讨论关于比如MSP430和cc3000的相关实验,我没搞明白,他们现在就用芯片做的板子呢还是在TI买的板子,然后就可以试着调试sdk的代码了吗,还是怎么回事?

    应该大部分是使用TI的EVM板进行评估的。建议您购买TI的EVM板进行评估。与CC3000相关的EVM板链接如下:https://estore.ti.com/Search.aspx?k=cc3000 

    2 如果是从TI拿到样片做出板子来调试的话,整个的板子的结构是什么样的呢?  TI网站上已经有了cc3000的连接图示,是不是就是拿MSP430的spi脚直接分别对应连上cc3000的spi对应管脚就ok了吗,还是怎么连接 ?

    除了SPI,主要还有芯片使能,中断信号等,根据您选定的EVM板,比如在上面链接中的一些EVM板。您可以直接在TI官网找到相关的MSP430和CC3000的参考设计的设计文件,您能够非常清晰的看出他们的连接方法。

    3 我下载MSP430的工具,填写好相关项后,点击submit,然后出现的页面是“这个页面打不开了”,或者“你访问的网页已经不存在了”。这个是真的打不开了,还是后台实际上已经提交ok了 ?

    您需要什么样的工具呢?应该不会出现这样的情况,MSP430是我们非常成熟的产品,应该不会有这样的问题。当然也有可能是您这边网络出现问题。您可以把需要的工具名和相关链接给我,我可以帮您试一下。

    4 如果3中描述的确实是网络问题,或者网页问题,烦请提供一份关于MSP430的sdk包给我一下。我的邮箱是  dushipingjlu@gmail.com

    根据您上面的需求,我会帮您落实。

    谢谢!

  • Shiping,

    另外,建议您以后将CC3000相关的问题发到我们的WIFI主题里,这样我们的WIFI专家会更快的发现并回复您的问题。谢谢!

    WIFI主题论坛链接:http://www.deyisupport.com/question_answer/wireless_connectivity/wifi/f/105.aspx