TI工程师您好,我想把cc3000应用到飞思卡尔上,现在有cc3000+msp430,如何实现呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
楼主,
如果是学习wifi的功能,CC3000是没问题的,如果是要做项目的话呢,建议还是采用CC3100或CC3200。因为这两款新片在性能,功耗方面有很大的优势。
要把CC3000和飞思卡尔的板子和在一起用,管家就是修改二者之间的接口定义和相关的SPI驱动的修改。我们的CC3000和MSP430之间主要通过四线的SPI然后再加一个GPIO和一个enable的使能信号。你可以在我们的SDK里的SPI.C和SPI.h以及board.c和board.h等相关的文件上做出修改。
关于SPI驱动的移植,你可以参考下面的wiki链接里的host guide相关的文档和网页信息:
http://processors.wiki.ti.com/index.php/CC3000
谢谢