This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

cc3000应用到飞思卡尔上

Other Parts Discussed in Thread: CC3100, CC3200

TI工程师您好,我想把cc3000应用到飞思卡尔上,现在有cc3000+msp430,如何实现呢?

  • shiyanshi,

    您好!

    建议您使用我们CC3000的升级产品CC3100产品:

    http://processors.wiki.ti.com/index.php/CC31xx_&_CC32xx?keyMatch=cc3100%20wiki&tisearch=Search-EN 

    使用也很简单,简单调用我们的API就能实现WIFI的相关功能,相关driver都在我们的CC3100 SDK里,参照我们example和文档来完成。谢谢!

  • 您好,主要我们已经购买了两套cc3000+msp430,那样这些就浪费了,cc3000应用到飞思卡尔上很困难吗?

  • 楼主,

       如果是学习wifi的功能,CC3000是没问题的,如果是要做项目的话呢,建议还是采用CC3100或CC3200。因为这两款新片在性能,功耗方面有很大的优势。

    要把CC3000和飞思卡尔的板子和在一起用,管家就是修改二者之间的接口定义和相关的SPI驱动的修改。我们的CC3000和MSP430之间主要通过四线的SPI然后再加一个GPIO和一个enable的使能信号。你可以在我们的SDK里的SPI.C和SPI.h以及board.c和board.h等相关的文件上做出修改。

       关于SPI驱动的移植,你可以参考下面的wiki链接里的host guide相关的文档和网页信息:

    http://processors.wiki.ti.com/index.php/CC3000

    谢谢