This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
通常会是硬件问题。你可以把模块飞线到一个TI的MCU板子上吗?像MSP430FR5739,就是在CC3000 WIKI上有参考设计的开发板。
然后可以验证一下CC3000MOD有没有问题。
您好,谢谢您的回答。
以上问题已经解决,是硬件问题,虚焊了。
现在已经可以和CC3000MOD通讯。但读取不到版本号?以下是测试的数据:
CC3000MOD和控制板通讯:
1、
Host ->> CC3000 - HCI_CMND_SIMPLE_LINK_START :0x01 0x00 0x05 0x00, 0x00 0x01 0x00 0x40 0x01 0x00
CC3000 ->> Host - HCI_EVNT_SIMPLE_LINK_START : 0X02 0X00 0X00 0X00 0X07 0X04 0X00 0X10 0X02 0X00(返回信息不对,代表着什么含义?是需要下载补丁包吗?)
2、
Host ->> CC3000 - HCI_CMND_SIMPLE_LINK_START :0x01 0x00 0x05 0x00, 0x00 0x01 0x00 0x40 0x01 0x02(把00改为02后,返回数据正常)
CC3000 ->> Host 能正常返回: 02 00 00 00 05 04 00 40 01 00
Host ->> CC3000 - HCI_CMND_READ_SP_VERSION :0x01 0x00 0x05 0x00 0x00 0x01 0x07 0x02 0x00 0x00
CC3000 ->> Host 返回:02 00 00 00 05 04 07 02 01 FF 02 00 00 00 (返回信息不对,代表着什么含义?)
以上问题,希望能帮忙解答一下,谢谢。