[ 216.265354] cfg80211: Loading compiled-in X.509 certificates for regulatory database
[ 216.333703] cfg80211: Loaded X.509 cert 'wens: 61c038651aabdcf94bd0ac7ff06c7248db18c600'
[ 216.342853] cfg80211: Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7'
[ 230.495979] cc33xx_sdio mmc2:0001:2: Using GPIO as IRQ
[ 230.503137] wlcore: cc33xx_probe :: Start
[ 230.503514] wlcore: Wireless Driver Version 1.7.0.127
[ 230.503673] cc33xx_driver cc33xx.4.auto: Direct firmware load for ti-connectivity/cc33xx-nvs.bin failed with error -2
[ 230.510276] wlcore: WLAN CC33xx platform device probe done
[ 230.514410] wlcore: Could not get nvs file ti-connectivity/cc33xx-nvs.bin
[ 230.514826] wlcore: Chip wakeup
[ 230.804583] wlcore: Set BLKsize to 128
[ 230.824636] wlcore: BOOT IRQs: 0x8
[ 232.832399] wlcore: Command T.O
[ 232.832420] wlcore: CMD# 35, len=712
[ 232.832431] wlcore: ERROR Device info command failure
[ 232.837656] wlcore: ERROR FW download failed
[ 232.856941] wlcore: wlcore_nvs_cb Complete