• CC3220R: MQTT无法连接,报错

    Part Number: CC3220R

    如图所示,SDK使用的版本为5.30.0.08版本,连接MQTT服务器时出现错误码-2005,请问这个错误码代表的是什么意思?我该如何修改我的工程?

  • CC3220R: CCS无法编译例程

    Part Number: CC3220R

    使用CCS12.3版本编译SDK5.3里面的MQTT例程,出现Error: SLImageCreator.exe: Device is not detected. The application binary was compiled, but the image cannot be generated. Plug in your LaunchPad and try again.请问如何解决?

  • CC3220R: 烧录报错:FS_ERROR_OFFSET_OUT_OF_RANGE

    Part Number: CC3220R
    Other Parts Discussed in Thread: CC3220S, , CC1350, UNIFLASH, CC3220SF

    自己的板上的CC3220R,用CC3220S的SDK开发。

    用CC1350的LaunchPad上的XDS调试(因为我没有CC3220R的LaunchPad,也没有标准XDS),调试运行都是一切正常的。

    但是当我想通过SLI文件下载到板子上时,出现了FS_ERROR_OFFSET_OUT_OF_RANGE的报错信息,具体截图如下…

  • CC3220SF-LAUNCHXL: CCS 打开CC3220SF例程,什么都没改,编译就有错,帮忙解决一下,谢谢好人

    Part Number: CC3220SF-LAUNCHXL
    Other Parts Discussed in Thread: CC3220SF, SYSBIOS

    我就打开例程然后编译,他就报错了,路径没中文没空格。网上找了几天了,救救我呗
    portable_CC3220SF_LAUNCHXL_tirtos_ccs:


    problems信息:
    Cannot build project. Referenced RTSC Configuration project 'tirtos_builds_CC3220SF_LAUNCHXL_release_ccs…

  • [FAQ] CC32XX系列sflash烧录指南

    Other Parts Discussed in Thread: UNIFLASH, CC3200MOD, CC3200

    CC32XX系列烧录sflash不能通过jtag,只能用UART或者SPI,具体步骤可参考芯片的production line guide。

     

    用JTAG无法把程序烧录进SFlash,必须使用串行接口,比如uniflash。假如想要debug并且把代码烧进flash,那两种接口都需要【注意相关的SOP设置】:

    • JTAG用于development,即debug
    • 串行接口用于把代…
  • imeter-boost

    Other Parts Discussed in Thread: CC3220SF, CC3200

    imeter boost那个测量电流和电压的GUI去哪里下载?

  • CC3220 和CC3235接camera sensor可以支持到多少像素?

    你好:

    CC3220 和CC3235都有8-bit camera接口,请问最大可以支持到多少像素?

  • 在例程中四条语句的作用是什么

    Other Parts Discussed in Thread: CC3220SF
            /* Initialize SlNetSock layer with CC3x20 interface                      */
            SlNetIf_init(0);
            SlNetIf_add(SLNETIF_ID_1, SLNET_IF_WIFI_NAME, (const SlNetIf_Config_t *)&SlNetIfConfigWifi, SLNET_IF_WIFI_PRIO);
            SlNetSock_init(0);
  • 使用cc3220sf作為mcu ,燒入器使用xds110來設計成自己的板子,需要做網址:http://dev.ti.com/tirex/explore/node?node=ALFqIj4dX6S.TZRERoSphA__FUz-xrs__LATEST中的Flashing the bootloader 設定pc才能找到xds110 comport嗎?

    使用cc3220sf作為mcu ,燒入器使用xds110來設計成自己的板子,需要做網址:http://dev.ti.com/tirex/explore/node?node=ALFqIj4dX6S.TZRERoSphA__FUz-xrs__LATEST中的Flashing the bootloader 設定pc才能找到xds110 comport嗎?就跟launchpad一樣,有圖文教學嗎?還是不需要做任何設定,自己做的板子插上usb連上pc後,pc就會自動找到xds110 comport了,就跟launchpad一樣…

  • 使用cc3220sf作為mcu ,燒入器使用xds110來設計成自己的板子,需要做圖中的設定嗎?有圖文詳細教學嗎?

    Other Parts Discussed in Thread: CC3220SF, UNIFLASH

    1.使用cc3220sf作為mcu ,燒入器使用xds110來設計成自己的板子,需要做圖中的設定嗎?有圖文詳細教學嗎?

    2.使用cc3220sf作為mcu ,燒入器使用xds110來設計成自己的板子,需要做網址:http://dev.ti.com/tirex/explore/node?node=ALFqIj4dX6S.TZRERoSphA__FUz-xrs__LATEST中的Flashing the…

  • 求CC3220SF在CCS及Uniflash上開發教學

    Other Parts Discussed in Thread: CC3220SF-LAUNCHXL, CC3200, SIMPLELINK-CC32XX-SDK, UNIFLASH, CC3220SF

    您好:

    我是CC3220SF-LAUNCHXL (SOP 跳線設置為 010)的初學者

    我的開發環境如下:

    Code Composer Studio         : CCS v9.1.0.00010

    CC3200 SDK                        :CC3200SDK-1.4.0-windows-inst…

  • CC3220s如何调整系统主频?

    Other Parts Discussed in Thread: CC1310, CC1350

    如上图以外的驱动如何获取API文档说明,而且上述文档的说明也不是很全,总感觉这个文档的输出属于乡镇企业的水平。

  • RE: 请问用CCS软件新建一个CC3220SF的工程,为什么工程里面没有启动文件?

     谢谢您的回答,我看CC3220的SDK里面给的demo里有基于FREERTOS和TIRTOS这样有操作系统的demo,还有基于NORTOS这样无操作系统的demo,我本来打算可以以操作底层寄存器的方式,编写源代码,来操作CC3220的,用CC3220来实现以太网、USB、485、无线Wi-Fi这几款通信协议的互相转换,但我看了NORTOS中的demo,如上图所示,想请教一下你们的NORTOS的demo虽然说是没有操作系统,但我感觉SDK里还是用了操作系统的思维在编写源代码?这样说是不是要想用CC3200实现我所说的上述通信协议转换功能…

  • RE: 请问用CCS软件新建一个CC3220SF的工程,为什么工程里面没有启动文件?

    我看了一下,MSP432这个类似于普通的MSP430类似包含了很多IRQ的注册以及时钟的启动使用。而CC3220的应用是建立在Freertos或者TI rtos的基础上,所以你CCS直接建立是无法完整建立,所以建议使用SDK里面的demo。
  • RE: 请问用CCS软件新建一个CC3220SF的工程,为什么工程里面没有启动文件?

    您好,谢谢回答,如图所示的打灰色背景的启动文件,我用CCS v8分别建立了一个CC3220和MSP432的工程,很奇怪为什么只有MSP432有启动文件,而CC3220没有?

  • RE: CC3220S linux 环境环境开发

    .out文件是可执行文件,可以用CCS jtag下载到CC3220里面执行,如果是用uniflash来烧录,需要hex或bin文件
  • CC3220 OTA

    使用cloud_ota demo 测试时,打开文件是失败Status=-10279

    OtaArchive_RunParseTar: parsing archive file header
    OtaArchive_RunParseTar: skip block align RecvBufLen=1440, SkipAlignSize=49
    OtaArchive_RunParseTar: FileType=0, FileName=/sys/mcubootinfo.bin, FileSize=16
    Create…

  • RE: 关于CC3220启动提示错误好可怕。。。。。

    估计是你没有配置对吧,导入官方例程的配置看看。
  • RE: 关于CC3220启动提示错误好可怕。。。。。

    此错误代码-2018 (= sl_ret_code_dev_not_start)仅在不启用NWP时返回。唯一可能的解释是sl_Stop()在代码中或在链接库中调用。
  • RE: 关于CC3220启动提示错误好可怕。。。。。

    /* The device has not been started yet */
    #define SL_RET_CODE_DEV_NOT_STARTED (-2018L)

    This error code -2018 (=SL_RET_CODE_DEV_NOT_STARTED) is returned only when NWP is not enabled. Only possible explanation is that…
  • 关于CC3220启动提示错误好可怕。。。。。

    line:24, error code:-2018] Device error, please refer "DEVICE ERRORS CODES" section in errors.h

    [line:24, error code:-2018] Device error, please refer "DEVICE ERRORS CODES" section in errors.h

    有谁知道是怎么回事

  • 【测评报告 C】 - 【TI CC3200-LAUNCHXL测评】工业物联网设备目标评估(二)—测试

    Other Parts Discussed in Thread: CC3200-LAUNCHXL, CC3200

    前文表述过,我对IOT WIFI解决方案更关心的是传输性能、易用性与扩展性,TI对CC3200特性的介绍显然超出我的预期,不错的性能(UPD 16Mbps、TCP 13Mbps),支持SmartConfig配网、RF自动校准以及丰富的外设接口都表明其作为IOT设备WIFI解决方案设计的勃勃雄心。下面仅针对CC3200-LAUNCHXL的TCP吞吐、SmartConfig配网以及与国密协处理器的扩展进行分析测试…

1 2 3 4 5 »