你好,我这边SDK使用08_30_01_01 ,协调器使用zc_thermostat_LP_CC1352P7_4_tirtos7_ticlang ,终端设备使用zed_temperaturesensor_LP_CC1352P7_4_tirtos7_ticlang。终端设备加入网络时一直处于zstack_DevState_DEV_END_DEVICE状态,像请教一下如何解决,或者协调器如何关闭信任认证功能。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,我这边SDK使用08_30_01_01 ,协调器使用zc_thermostat_LP_CC1352P7_4_tirtos7_ticlang ,终端设备使用zed_temperaturesensor_LP_CC1352P7_4_tirtos7_ticlang。终端设备加入网络时一直处于zstack_DevState_DEV_END_DEVICE状态,像请教一下如何解决,或者协调器如何关闭信任认证功能。
zstack_DevState_DEV_END_DEVICE是已加入网络的终端设备的正确状态。
/** * Device States for the Network Information Read response (@ref * zstack_sysNwkInfoReadRsp_t) and the * Device State Change indication (@ref zstack_devStateChangeInd_t). */ typedef enum { /** Initialized - not started automatically */ zstack_DevState_HOLD = 0, /** Initialized - not connected to anything */ zstack_DevState_INIT = 1, /** Discovering PAN's to join */ zstack_DevState_NWK_DISC = 2, /** Joining a PAN */ zstack_DevState_NWK_JOINING = 3, /** * ReJoining a PAN in secure mode scanning in current channel, * only for end devices */ zstack_DevState_NWK_REJOIN_SEC_CURR_CHANNEL = 4, /** Joined but not yet authenticated by trust center */ zstack_DevState_END_DEVICE_UNAUTH = 5, /** Started as device after authentication */ zstack_DevState_DEV_END_DEVICE = 6, /** Device joined, authenticated and is a router */ zstack_DevState_DEV_ROUTER = 7, /** Started as Zigbee Coordinator */ zstack_DevState_COORD_STARTING = 8, /** Started as Zigbee Coordinator */ zstack_DevState_DEV_ZB_COORD = 9, /** Device has lost information about its parent */ zstack_DevState_NWK_ORPHAN = 10, /** Device is sending KeepAlive message to its parent */ zstack_DevState_NWK_KA = 11, /** Device is waiting before trying to rejoin */ zstack_DevState_NWK_BACKOFF = 12, /** * ReJoining a PAN in secure mode scanning in all channels, * only for end devices */ zstack_DevState_NWK_REJOIN_SEC_ALL_CHANNEL = 13, /** * ReJoining a PAN in unsecure mode scanning in current channel, * only for end devices */ zstack_DevState_NWK_TC_REJOIN_CURR_CHANNEL = 14, /** * ReJoining a PAN in unsecure mode scanning in all channels, * only for end devices */ zstack_DevState_NWK_TC_REJOIN_ALL_CHANNEL = 15, } zstack_DevState;
我不知道如何进一步协助,因为这不是问题。如果ZC将BDB_DEFAULT_TC_REQUIRE_KEY_EXCHANGE设置为FALSE,则ZED也可以将requestNewTrustCenterLinkKey设置为FALSE,然后在加入后不请求新的信任中心链接密钥。