由于mcu的管脚都被占用了,只剩下串口了。
想问下,PM2能支持串口唤醒吗?如果不能,那么哪个休眠能支持串口呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
由于mcu的管脚都被占用了,只剩下串口了。
想问下,PM2能支持串口唤醒吗?如果不能,那么哪个休眠能支持串口呢?
这我看过了,我按照他的方法做
在hal_board_cfg.h里改
#define HAL_UART_ISR 1
#define HAL_UART_DMA 0
在SampleApp.c中休眠前加入
// 配置串口为普通的GPIO
P0SEL &= ~0X20; //外P0_5为通用接口模式
P0DIR &= ~0X20; //P0_5为输入
P0IEN |= 0X20; //开P0_5的IO中断使能
IEN1 |= 0X20; //开P0的中断
// end
在唤醒后加入
// 恢复串口
P0SEL = 0x3C;
P0DIR = 0X01;
P0IEN = 0X00;
IEN1 = 0X04;
// end
然后测试后还是不行,调试发现,是用的ISR模式,唤醒前P0的中断函数正常。
进入休眠后,有数据过来没有P0中断,有没有可能是和我的按键P0_4冲突了?