This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

2530能否用串口唤醒休眠

由于mcu的管脚都被占用了,只剩下串口了。

想问下,PM2能支持串口唤醒吗?如果不能,那么哪个休眠能支持串口呢?

  • 论坛有类似问题,解答请看这边: https://www.deyisupport.com/question_answer/wireless_connectivity/zigbee/f/104/t/65755.aspx

  • 这我看过了,我按照他的方法做

    在hal_board_cfg.h里改

    #define HAL_UART_ISR 1
    #define HAL_UART_DMA 0

    在SampleApp.c中休眠前加入

    // 配置串口为普通的GPIO
    P0SEL &= ~0X20; //外P0_5为通用接口模式
    P0DIR &= ~0X20; //P0_5为输入
    P0IEN |= 0X20; //开P0_5的IO中断使能
    IEN1 |= 0X20; //开P0的中断
    // end

    在唤醒后加入

    // 恢复串口
    P0SEL = 0x3C;
    P0DIR = 0X01;
    P0IEN = 0X00;
    IEN1 = 0X04;
    // end

    然后测试后还是不行,调试发现,是用的ISR模式,唤醒前P0的中断函数正常。
    进入休眠后,有数据过来没有P0中断,有没有可能是和我的按键P0_4冲突了?