终端掉线后(协调器断电)然后协调器上电,终端rejoin一直发beacon request,无法恢复入网,我预编译了NV_RESTORE,怎么回事呀?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
发送完beacon request以后,如果协调器有回beacon的话,节点会调用到ZDO_beaconNotifyIndCB( NLME_beaconInd_t *pBeacon ),
可以单步调试下有没有把获取到的网络信息,放到NwkDescList里面去。
然后去下面的代码,有没有运行到
case ZDO_NWK_DISC_CNF:
if (devState != DEV_NWK_DISC)
break;
if ( ZG_BUILD_JOINING_TYPE && ZG_DEVICE_JOINING_TYPE )
{
// Process the network discovery scan results and choose a parent
// device to join/rejoin itself
networkDesc_t *pChosenNwk;
if ( ( (pChosenNwk = ZDApp_NwkDescListProcessing()) != NULL )VV
我这边发现,寻网的终端 在 进入到 PredevState == DEV_NWK_SEC_REJOIN_ALL_CHANNEL 的时候,
会有 清NWK 的操作。。。请问 这个会不会导致清除之后
开启Start the reset timer for MAX UNAUTH time ,然后 MAX_DEVICE_UNAUTH_TIMEOUT 这段时间内 由于外界的因素 又没能 收到新的NWK key
设备就把NV flash 里面的东西删除, 接着就入不了网,也就是systemreset。(此时即便是有beacon ,但是设备NV flash 里面的信息被复位擦除了,只能开permit join 才能入网,无论哪个协调器!!!)
else if ( devState == DEV_NWK_ORPHAN ||
<strong><span style="color:#ff0000;">devState == DEV_NWK_SEC_REJOIN_CURR_CHANNEL</span></strong> ||
devState == DEV_NWK_TC_REJOIN_CURR_CHANNEL ||
devState == DEV_NWK_TC_REJOIN_ALL_CHANNEL ||
devState == DEV_NWK_SEC_REJOIN_ALL_CHANNEL )
{
......................
// results of an orphaning attempt by this device
// results of an orphaning attempt by this device
<strong><span style="color:#ff0000;"> if (nwkStatus == ZSuccess)</span></strong>
{
//When the device has successfully rejoined then reset retryCnt
retryCnt = 0;
// Verify NWK key is available before sending Device_annce
if ( ZG_SECURE_ENABLED && ( ZDApp_RestoreNwkKey( TRUE ) == false ) )
{
// wait for auth from trust center
ZDApp_ChangeState( DEV_END_DEVICE_UNAUTH );
// Start the reset timer for MAX UNAUTH time
ZDApp_ResetTimerStart( MAX_DEVICE_UNAUTH_TIMEOUT );
}