This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SmartRF Flash Programmer 烧写问题

各位好,

            我使用SmartRF Flash Programmer 给2530烧写程序,按照网上的说明修改了设置以及去掉了f8w2530.xcl里的两行注释,烧写协调器程序时出现下面问题,烧写路由程序和终端程序没有问题,可以在IAR debug模式下烧写协调器程序,但是这样为以后生产带来不便,

请问这个问题我如何解决?谢谢指教。

  • 请问IAR内是如何设置生成hex文件的?

  • 你好,

             IAR内设置如下图,在f8w2530.xcl里去掉了如下两行的注释,请问还有什么需要修改设置的地方么?我的路由节点按照这种方式生成的hex文件能正常烧写到2530里。

    ////编译hex去掉两行的注释
    // Include these two lines when generating a .hex file for banked code model:
    -M(CODE)[(_CODEBANK_START+_FIRST_BANK_ADDR)-(_CODEBANK_END+_FIRST_BANK_ADDR)]*\
    _NR_OF_BANKS+_FIRST_BANK_ADDR=0x8000