尊敬的IT大神们: zigbee协议栈中,为什么我配置15信道,路由都不能入网,其他的信道就可以,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
//-DMAX_CHANNELS_868MHZ 0x00000001
//-DMAX_CHANNELS_915MHZ 0x000007FE
//-DMAX_CHANNELS_24GHZ 0x07FFF800
//-DDEFAULT_CHANLIST=0x04000000 // 26 - 0x1A
//-DDEFAULT_CHANLIST=0x02000000 // 25 - 0x19
//-DDEFAULT_CHANLIST=0x01000000 // 24 - 0x18
//-DDEFAULT_CHANLIST=0x00800000 // 23 - 0x17
//-DDEFAULT_CHANLIST=0x00400000 // 22 - 0x16
//-DDEFAULT_CHANLIST=0x00200000 // 21 - 0x15
//-DDEFAULT_CHANLIST=0x00100000 // 20 - 0x14
//-DDEFAULT_CHANLIST=0x00080000 // 19 - 0x13
//-DDEFAULT_CHANLIST=0x00040000 // 18 - 0x12
//-DDEFAULT_CHANLIST=0x00020000 // 17 - 0x11
//-DDEFAULT_CHANLIST=0x00010000 // 16 - 0x10
//-DDEFAULT_CHANLIST=0x00008000 // 15 - 0x0F
//-DDEFAULT_CHANLIST=0x00004000 // 14 - 0x0E
//-DDEFAULT_CHANLIST=0x00002000 // 13 - 0x0D
//-DDEFAULT_CHANLIST=0x00001000 // 12 - 0x0C
//-DDEFAULT_CHANLIST=0x00000800 // 11 - 0x11
//11,15,16,19,20,21,22,23
-DDEFAULT_CHANLIST=0x00008000 // 20 - 0x14
//-DDEFAULT_CHANLIST=0x00ff0800 // 20 - 0x14
这样配置15信道对吗??