This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

zigbee 信道

尊敬的IT大神们: zigbee协议栈中,为什么我配置15信道,路由都不能入网,其他的信道就可以,

  • 参考这边信道设置,看看步骤/数值是否正确

  • //-DMAX_CHANNELS_868MHZ 0x00000001
    //-DMAX_CHANNELS_915MHZ 0x000007FE
    //-DMAX_CHANNELS_24GHZ 0x07FFF800
    //-DDEFAULT_CHANLIST=0x04000000 // 26 - 0x1A
    //-DDEFAULT_CHANLIST=0x02000000 // 25 - 0x19
    //-DDEFAULT_CHANLIST=0x01000000 // 24 - 0x18
    //-DDEFAULT_CHANLIST=0x00800000 // 23 - 0x17
    //-DDEFAULT_CHANLIST=0x00400000 // 22 - 0x16
    //-DDEFAULT_CHANLIST=0x00200000 // 21 - 0x15
    //-DDEFAULT_CHANLIST=0x00100000 // 20 - 0x14
    //-DDEFAULT_CHANLIST=0x00080000 // 19 - 0x13
    //-DDEFAULT_CHANLIST=0x00040000 // 18 - 0x12
    //-DDEFAULT_CHANLIST=0x00020000 // 17 - 0x11
    //-DDEFAULT_CHANLIST=0x00010000 // 16 - 0x10
    //-DDEFAULT_CHANLIST=0x00008000 // 15 - 0x0F
    //-DDEFAULT_CHANLIST=0x00004000 // 14 - 0x0E
    //-DDEFAULT_CHANLIST=0x00002000 // 13 - 0x0D
    //-DDEFAULT_CHANLIST=0x00001000 // 12 - 0x0C
    //-DDEFAULT_CHANLIST=0x00000800 // 11 - 0x11
    //11,15,16,19,20,21,22,23

    -DDEFAULT_CHANLIST=0x00008000 // 20 - 0x14
    //-DDEFAULT_CHANLIST=0x00ff0800 // 20 - 0x14

    这样配置15信道对吗??