在CC2530的基础上加了CC2591,没有加CC2591的一个版本通讯距离(0dbm)是13米左右,加了CC2591之后,通讯距离去只有几十厘米,怎么判断我加了CC2591的硬件没有错呢?我用Smart RF studio验证了没有CC2591和有CC2591的板子,结果有CC2591的选项,不知道怎么回事。。。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,感谢您的回答。软件里面也是改了的。#define HAL_PA_LNA,
#if defined (HAL_PA_LNA)
const uint8 CODE macRadioDefsTxPowerTable[] =
{
/* 0 dBm */ 0x05, /* TBD: place holder */ /*都是0xD5*/
/* 1 dBm */ 0x15, /* TBD: place holder */
/* 2 dBm */ 0x25, /* TBD: place holder */
/* 3 dBm */ 0x25, /* TBD: place holder */
/* 4 dBm */ 0x35, /* TBD: place holder */
/* 5 dBm */ 0x35, /* TBD: place holder */
/* 6 dBm */ 0x45, /* TBD: place holder */
/* 7 dBm */ 0x45, /* TBD: place holder */
/* 8 dBm */ 0x55, /* TBD: place holder */
/* 9 dBm */ 0x55, /* TBD: place holder */
/* 10 dBm */ 0x55, /* TBD: place holder */
/* 11 dBm */ 0x65, /* TBD: place holder */
/* 12 dBm */ 0x75, /* TBD: place holder */
/* 13 dBm */ 0x75, /* TBD: place holder */
/* 14 dBm */ 0x85, /* TBD: place holder */
/* 15 dBm */ 0x95, /* TBD: place holder */
/* 16 dBm */ 0xA5, /* TBD: place holder */
/* 17 dBm */ 0xB5, /* TBD: place holder */
/* 18 dBm */ 0xD5, /* TBD: place holder */
/* 19 dBm */ 0xF5 /* TBD: place holder */
};
有篇文章http://www.ti.com/lit/an/swra308a/swra308a.pdf
软件就按照8 Controlling the CC2591章节去改就好了。
BR.AZ
您好,谢谢您的回复,问题已经解决,主要是32MHz和32Khz时钟没有同步引起的