Other Parts Discussed in Thread: CC2530
描述:
1、CC2530 非开发套件,使用 SampleDoorLock 作为协调器、SampleDoorLockController作用终端
2、终端(SampleDoorLockController)开启一个定时器来检测按键(100ms),例如:P1_5 ==1时,来发起Becon reques 请求并且可以入网(入网抓包如下图)
3、例如:P1_6 ==1时,来发送解锁命令,但是数据发来出来,抢包没有抢出来。debug能正常进入定时器检测,例程其他地方没有改动,请问问题出在那里呢?谢谢,代码如下:
if ( events & SAMPLEDOORLOCK_wds )
{
osal_start_timerEx( zclSampleDoorLockController_TaskID, SAMPLEDOORLOCK_wds, 100 );
// zcl_EZModeAction ( EZMODE_ACTION_TIMED_OUT, NULL ); // EZ-Mode timed out
if(P1_6==1)
{
// increase PIN number
if ( giDoorLockScreenMode == DOORLOCK_PINMODE )
{
if ( giDoorLockPINColumnCount < 4 )
{
if ( giDoorLockPINCount > 8 )
{
giDoorLockPINCount = 0;
}
else
{
giDoorLockPINCount++;
}
}
}
// for all other modes, lock/unlock door
else
{
zclDoorLock_t cmd;
cmd.pPinRfidCode = aiDoorLockPIN;
static bool locked = TRUE;
giDoorLockScreenMode = DOORLOCK_MAINMODE;
if ( locked )
{
zclClosures_SendDoorLockUnlockDoor( SAMPLEDOORLOCKCONTROLLER_ENDPOINT, &zclSampleDoorLockController_DstAddr, &cmd, false, zclSampleDoorLockControllerSeqNum++ );
locked = FALSE;
}
else
{
zclClosures_SendDoorLockLockDoor( SAMPLEDOORLOCKCONTROLLER_ENDPOINT, &zclSampleDoorLockController_DstAddr, &cmd, false, zclSampleDoorLockControllerSeqNum++ );
locked = TRUE;
}
}
}
if(P1_5==1)
{
if ( ( giDoorLockScreenMode == DOORLOCK_MAINMODE ) ||
( giDoorLockScreenMode == DOORLOCK_HELPMODE ) )
{
giDoorLockScreenMode = DOORLOCK_MAINMODE;
#ifdef ZCL_EZMODE
{
zclEZMode_InvokeData_t ezModeData;
static uint16 clusterIDs[] = { ZCL_CLUSTER_ID_CLOSURES_DOOR_LOCK }; // only bind on the on/off cluster
// Invoke EZ-Mode
ezModeData.endpoint = SAMPLEDOORLOCKCONTROLLER_ENDPOINT; // endpoint on which to invoke EZ-Mode
if ( ( zclSampleDoorLockController_NwkState == DEV_ZB_COORD ) ||
( zclSampleDoorLockController_NwkState == DEV_ROUTER ) ||
( zclSampleDoorLockController_NwkState == DEV_END_DEVICE ) )
{
ezModeData.onNetwork = TRUE; // node is already on the network
}
else
{
ezModeData.onNetwork = FALSE; // node is not yet on the network
}
ezModeData.initiator = TRUE; // DoorLock Controller is an initiator
ezModeData.numActiveInClusters = 0;
ezModeData.pActiveInClusterIDs = NULL;
ezModeData.numActiveOutClusters = 1; // active output cluster
ezModeData.pActiveOutClusterIDs = clusterIDs;
zcl_InvokeEZMode( &ezModeData );
#ifdef LCD_SUPPORTED
HalLcdWriteString( "EZMode", HAL_LCD_LINE_2 );
#endif
}
// NOT ZCL_EZMODE, Use EndDeviceBind
#else
{
zAddrType_t dstAddr;
HalLedSet ( HAL_LED_4, HAL_LED_MODE_OFF );
// Initiate an End Device Bind Request, this bind request will
// only use a cluster list that is important to binding.
dstAddr.addrMode = afAddr16Bit;
dstAddr.addr.shortAddr = 0; // Coordinator makes the match
ZDP_EndDeviceBindReq( &dstAddr, NLME_GetShortAddr(),
SAMPLEDOORLOCKCONTROLLER_ENDPOINT,
ZCL_HA_PROFILE_ID,
0, NULL, // No incoming clusters to bind
ZCLSAMPLEDOORLOCKCONTROLLER_BINDINGLIST, bindingOutClusters,
TRUE );
}
#endif // ZCL_EZMODE
}
}
return ( events ^ SAMPLEDOORLOCK_wds );
}