Other Parts Discussed in Thread: CC2538, CC2530, Z-STACK
您好:
cc2538(当协调器)和cc2530(当终端)进行简单的无线通讯时,双方使用的都是基于mesh协议栈的,一开始通讯没问题,但当通讯几个小时后无线通讯会断且不能自己恢复,必须手动重启其中一个或两个才能恢复通讯,拷机测试了n多次都是这个现象。(使用的都是mesh包里的GeneralApp工程)
麻烦可以帮忙解决一下。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
【三木电子科技有限公司厂家直销店】
点击链接,再选择浏览器打开;或复制这条信息€ifTl0Eidy8l€后打开淘宝
这是2538的链接。
【CC2530开发套件 zigbee开发板无线模块 wifi安卓 物联网智能家居】,复制这条信息¥QXb40vaEKKA¥后打开手淘
这是2530的链接。
而且我昨天试了用两个2530进行通讯,一个作为协调器,一个作为终端,其中一个2530广播,另外一个2530收到数据再单播。没有出现通讯断起不来的情况。
是的,我之前用两个2530测试没通讯断时,我也是怀疑2538有问题。所以买个2538回来验证下是不是2538问题,发现还是没有正常。
您那边能提供hex麽,我怕是IAR环境的问题。
哥您好,我现在这边2538当协调器,2530当终端还是不行的。
但是,我反过来后就是把2530当协调器,2538当终端就可以的,不会出现通讯断的现象,不知道这是为什么的?