Other Parts Discussed in Thread: UNIFLASH, CC2652R, CC2650
CCS7.4,CC26x2 1.6 SDK
CC2652R使用Zstack 1.6 插件和1.6的SDK,uniflash完全擦除flash然后调试,能通过ICall_createRemoteTasks,第二次调试,也能进入main,但运行到ICall_createRemoteTasks就卡住了,没有代码,没办法进一步的调试,如何处理?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我这边没有用官方的板子,是第三方的板子,更换的CC2652R芯片,可以正常使用,读取IEEE地址,都正常,说明板子没有问题。
debug也能debug,能进入main入口,不是说一点都运行不了,问题就是运行到ICall_createRemoteTasks就卡住了,详细调试之后发现具体是卡在了Task_restore这个函数的位置,没有源代码,不知道什么问题造成的。
帮忙debug一下,看看keytask变量在Task_disable函数调用之后的返回值是多少,是不是0,因为后面卡在Task_restore,我怀疑是这一块代码实现有问题。
/* See header file for comments */
void ICall_createRemoteTasks(void)
{
size_t i;
UInt keytask;
/* Cheap locking mechanism to lock tasks
* which may attempt to access the service call dispatcher
* till all services are registered.
*/
keytask = Task_disable();
for (i = 0; i < ICALL_REMOTE_THREAD_COUNT; i++)
{
Task_Params params;
Task_Handle task;
ICall_CSState key;
Task_Params_init(¶ms);
params.priority = ICall_threadPriorities[i];
params.stackSize = ICall_threadStackSizes[i];
params.arg0 = (UArg) icall_threadEntries[i];
params.arg1 = (UArg) ICall_getInitParams(i);
task = Task_create(ICall_taskEntry, ¶ms, NULL);
if (task == NULL)
{
/* abort */
ICALL_HOOK_ABORT_FUNC();
}
key = ICall_enterCSImpl();
if (ICall_newTask(task) == NULL)
{
/* abort */
ICALL_HOOK_ABORT_FUNC();
}
ICall_leaveCSImpl(key);
}
Task_restore(keytask);
}
另外,点击以下小锤子编译,没有一分钟都编译不完,有这么慢吗,又不是全部编译
我尝试在里面点亮一颗LED,直接烧录hex文件也无法启动,我不认为是硬件问题,既然IEEE地址都可以读取,并且uniflash load image都没问题,说明硬件是可以正常的,不然别的地方都不卡住,就卡在这个地方,而且最主要的是还没有源代码,不清楚这里面到底干了什么事情。
见过那种硬件有问题的,JTEG都连不上。
如果硬件有问题,比如晶振无法启震,芯片引脚短路等等,JTEG都会连不上,更别说erase flash,读取IEEE地址,读取MEMORY都正常。
关键是debug时候还能进入main入口,并且一步一步运行到ICall_createRemoteTasks并卡死,中途查看其他变量,看起来初始化都还算正常。
以前的OSAL也会在启动的时候卡住在Mac_Init初始化的位置,后来跟踪进去发现是使用了外部32.768Khz晶振,没有起震,导致卡住,现在这个TI-RTOS不一样,中间多了一层叫做Icall的middleware中间件,很多都密封进库里面,也看不到,也无法调试,更是无从知道问题出在哪里了。
我很怀疑编译出来的firmware有问题,附件我上传了一个默认的条件编译出来的zed_switch_cc26x2lp.hex和zed_switch_cc26x2lp.out,以及stack映射文件zed_switch_cc26x2lp.map。
另外你那边能否帮忙编译个.hex,点亮RED(当前默认是GIO6引脚)这颗LED,我过来烧写进去看看能否点亮?
/*******************************************************************************
* @fn zclSampleSw_initialization
*
* @brief Initialize the application
*
* @param none
*
* @return none
*/
static void zclSampleSw_initialization(void)
{
/* Initialize user clocks */
zclSampleSw_initializeClocks();
/* Initialize keys */
Board_Key_initialize(zclSampleSw_changeKeyCallback);
/* Initialize the LEDS */
Board_Led_initialize();
// Register the current thread as an ICall dispatcher application
// so that the application can send and receive messages.
ICall_registerApp(&zclSampleSw_Entity, &sem);
//Initialize stack
zclSampleSw_Init();
Board_Led_control(board_led_type_LED1,board_led_state_ON);
}
我烧写你那个hex文件 led不亮的。
我自己加了那段代码:
static void zclSampleSw_initialization(void)
{
/* Initialize user clocks */
zclSampleSw_initializeClocks();
/* Initialize keys */
Board_Key_initialize(zclSampleSw_changeKeyCallback);
/* Initialize the LEDS */
Board_Led_initialize();
// Register the current thread as an ICall dispatcher application
// so that the application can send and receive messages.
ICall_registerApp(&zclSampleSw_Entity, &sem);
Board_Led_control(board_led_type_LED1, board_led_state_ON);
//Initialize stack
zclSampleSw_Init();
}
你烧写一下我的那个hex文件是可以点亮的。
https://e2echina.ti.com/cfs-file/__key/communityserver-discussions-components-files/104/zc_5F00_switch_5F00_cc26x2lp.7z
重新更换了一个新的CC2652R,你给的固件烧进去,连接在GPIO6上的红色LED终于点亮了。
没有买TI的LaunchPad开发板(开发板上带了一堆没用的东西,还卖的较贵),其实没必要为SmartEnergy和LaunchPad上带的下载器重复花钱,都有外接下载器,还要每个LaunchPad上自带一个,完全没必要,只能提高成本。
现在世面上任何一家CC2650的模块,只要把芯片换成CC2652R,另外换掉原来的24M晶振,换成48M的,就直接可以点亮了,RGZ封装的引脚都是完全兼容的,目前debug模式下XDS100 V3的确会有问题,会卡在ICall_createRemoteTasks不能往下走,目前手头没有XDS200的下载器,没办法做进一步的测试。
另外不知是CCS7.4,还是TI的编译器,似乎是有bug的,有时候稍微修改几行代码,Build project出来的hex烧进去运行不了,回头重新执行Rebuild project,等了很久,出来的hex固件烧进去反而运行正常。不是很可靠,理论上修改代码不会影响到project的配置,不应该出现这种情况,之前IAR for ARM/8051从来没遇到过类似问题。
然后我这边重新编译新的固件,都能点亮LED,blink也都正常,说明RTOS最起码跑起来了,刚刚测试了一下zed_switch看能不能入网,修改了CC26X2R1_LAUNCHXL.c里面gpioPinConfigs的引脚配置,可以支持当前平台的按键了,
虽然按键已经调用steering,但似乎没办法发出beacon request请求入网。很奇怪,就算network key不对,最起码能发出beacon request才对,但是ubiqua在默认的11信道抓包没有。
zstack_bdbStartCommissioningReq.commissioning_mode = BDB_COMMISSIONING_MODE_NWK_STEERING/* | BDB_COMMISSIONING_MODE_FINDING_BINDING*/;
Zstackapi_bdbStartCommissioningReq(zclSampleSw_Entity,&zstack_bdbStartCommissioningReq);
目前simplelink_zigbee_sdk_plugin_1_60_00_14.exe的确默认是11信道,还不清楚是哪里问题。
/* Default channel is Channel 11 - 0x0B */ // Channels are defined in the following: // 0 : 868 MHz 0x00000001 // 1 - 10 : 915 MHz 0x000007FE // 11 - 26 : 2.4 GHz 0x07FFF800 // //#define MAX_CHANNELS_868MHZ 0x00000001 //#define MAX_CHANNELS_915MHZ 0x000007FE //#define MAX_CHANNELS_24GHZ 0x07FFF800 //#define DEFAULT_CHANLIST 0x04000000 // 26 - 0x1A //#define DEFAULT_CHANLIST 0x02000000 // 25 - 0x19 //#define DEFAULT_CHANLIST 0x01000000 // 24 - 0x18 //#define DEFAULT_CHANLIST 0x00800000 // 23 - 0x17 //#define DEFAULT_CHANLIST 0x00400000 // 22 - 0x16 //#define DEFAULT_CHANLIST 0x00200000 // 21 - 0x15 //#define DEFAULT_CHANLIST 0x00100000 // 20 - 0x14 //#define DEFAULT_CHANLIST 0x00080000 // 19 - 0x13 //#define DEFAULT_CHANLIST 0x00040000 // 18 - 0x12 //#define DEFAULT_CHANLIST 0x00020000 // 17 - 0x11 //#define DEFAULT_CHANLIST 0x00010000 // 16 - 0x10 //#define DEFAULT_CHANLIST 0x00008000 // 15 - 0x0F //#define DEFAULT_CHANLIST 0x00004000 // 14 - 0x0E //#define DEFAULT_CHANLIST 0x00002000 // 13 - 0x0D //#define DEFAULT_CHANLIST 0x00001000 // 12 - 0x0C #define DEFAULT_CHANLIST 0x00000800 // 11 - 0x0B
为了方便您的测试,我把建立网络写在了初始化中。
zstack_bdbStartCommissioningReq_t zstack_bdbStartCommissioningReq;
zstack_bdbStartCommissioningReq.commissioning_mode = BDB_COMMISSIONING_MODE_NWK_FORMATION | BDB_COMMISSIONING_MODE_NWK_STEERING;
Zstackapi_bdbStartCommissioningReq(zclSampleSw_Entity,&zstack_bdbStartCommissioningReq);
UI_UpdateLcd();
附件中为固件,您下载之前请All Unprotected Sectors。https://e2echina.ti.com/cfs-file/__key/communityserver-discussions-components-files/104/8877.zc_5F00_switch_5F00_cc26x2lp.7z
Alvin,
今天多谢你的支持,不能发出beacon request的问题终于找到了,CC2652R LaunchPad参考设计48M晶振外部是没有两颗负载电容的,经过查看手册,是芯片内置了负载电容,所以我买的模块也没外接电容,但是预留有位置,我尝试焊了两个7pf的电容上去,我的zed firmware,你的zc firmware,都能发出beacon request了。
至此,完全正常运行,但是XDS100 V3 debug仍然会卡在ICall_createRemoteTasks,可能要换XDS110或者XDS200再试试了。
这个原因一大部分可能是晶振的负载电容不恰当,导致起震频率不正确,最终导致倍频后2.4G RF偏频,所以即使ubiqua在11信道抓包,但是芯片发出的频率其实不是真正的11信道频率,自然就无法抓到包了。
我开始就怀疑是频点不对,所以无法抓到包。但我手头又没有频谱仪,无从判断。
总结下来,再次提醒后面要在CC2652R上做硬件设计的朋友,48M的晶振,如此之高,鄙人见识少,多年来实属罕见。原理图设计一定要预留两颗负载电容的设计,以备不时之需,看来外接晶振要有负载电容千年不变的真理。