This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2652R zed_switch工程定义了POWER_SAVING宏仍然是8mA电流 无法休眠

Other Parts Discussed in Thread: CC2652R, TPS63031, TPS62730

1.6SDK版本,

是不是需要额外设置什么,默认的zed_switch工程,入网成功以后,似乎无法进入休眠?经测试,8mA电流消耗很稳定。

  • 你是用TI LAUNCHXL-CC2652测試的嗎?

  • 不是,是cc2652r模块无外设,已经入网成功,控制都没问题,然后直接测试的电流,是8ma,很长时间都是,显然没有进入休眠,不知Launch板子上是否同样无法进入休眠? 手头没有板子无法测试

  • 我記得之前測試看到的修眠電流大概是8-10uA.
  • 在LAUNCHXL-CC2652上测试能进入休眠,电流在几个uA
  • 建議檢查看看你的IO有沒有在漏電

  • 原来是外部的boost DCDC TPS63031静态功耗很高,起始已经进入休眠状态了,功耗只有1.2uA左右很稳定,看来最新的CC2652R的确是功耗很低,适合纽扣电池供电。
  • CC26XX测试功耗其实都可以参照下面的BLE测试手册,特别是当你使用的是Launchpad的时候外部接线是一样的原理。
    www.ti.com.cn/.../zhca712c.pdf
  • 主要是DCDC这一块选型有点问题。
    现在功耗已经很低很低了,实测1.2uA左右,基本上按键唤醒后,立即会进入深度休眠模式,现在改为1分钟data request一次,估计也比较费电。
    为什么两节干电池供电已经是3V了,还要DCDC,早先的MCU由于所需最低电压一般都在2V,如果两节干电池供电的话,在电压较低时可能会带不起来,加上DCDC稍微升压一下,会延长电池使用寿命。

    但是现在看CC2652R规格书,最低电压已经能到1.8V了,显然比TPS62730的最低启动电压还要低,基本上能把干电池充分使用了。要不要DCDC基本没什么用,还多几块钱的成本。


    像TPS62730这种带有旁路功能的DCDC才适合这种方式,MCU控制TPS62730其中一个引脚,休眠时拉低,直接bypass,用电池供电,唤醒时拉高,启动DCDC,目的只是为了升压,延长电池的使用寿命。
    一般的DCDC,EN脚只要拉低,后面的MCU就无法供电只能关机了。