Other Parts Discussed in Thread: CC2652R, TPS63031, TPS62730
1.6SDK版本,
是不是需要额外设置什么,默认的zed_switch工程,入网成功以后,似乎无法进入休眠?经测试,8mA电流消耗很稳定。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
主要是DCDC这一块选型有点问题。
现在功耗已经很低很低了,实测1.2uA左右,基本上按键唤醒后,立即会进入深度休眠模式,现在改为1分钟data request一次,估计也比较费电。
为什么两节干电池供电已经是3V了,还要DCDC,早先的MCU由于所需最低电压一般都在2V,如果两节干电池供电的话,在电压较低时可能会带不起来,加上DCDC稍微升压一下,会延长电池使用寿命。
但是现在看CC2652R规格书,最低电压已经能到1.8V了,显然比TPS62730的最低启动电压还要低,基本上能把干电池充分使用了。要不要DCDC基本没什么用,还多几块钱的成本。
像TPS62730这种带有旁路功能的DCDC才适合这种方式,MCU控制TPS62730其中一个引脚,休眠时拉低,直接bypass,用电池供电,唤醒时拉高,启动DCDC,目的只是为了升压,延长电池的使用寿命。
一般的DCDC,EN脚只要拉低,后面的MCU就无法供电只能关机了。