This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ZED poll rate set incorrectly if reset from a leave request with rejoin enabled 究竟是怎样改?不是很明白

Genius 3030 points


ZED poll rate set incorrectly if reset from a leave request with rejoin enabled

Issue description:
ZED will poll using REJOIN_POLL_RATE instead of POLL_RATE after being reset due to a parent leave request where the rejoin option was set.

Proposed fix:
In ZDApp_ProcessNetworkJoin of ZDApp.c, remove NLME_SetPollRate( zgRejoinPollRate ); from if (nwkStatus == ZSuccess) and place in the else statement instead. One must also set the zgRejoinPollRate when device state is DEV_END_DEVICE_UNAUTH

if ( ZG_SECURE_ENABLED && ( ZDApp_RestoreNwkKey( TRUE ) == false ) )
{
  if ( ZSTACK_END_DEVICE_BUILD )
  {
     NLME_SetPollRate( zgRejoinPollRate );
  }
  // wait for auth from trust center
  ZDApp_ChangeState( DEV_END_DEVICE_UNAUTH );

Optimally, also place NLME_SetPollRate( ZDApp_SavedPollRate ); inside of ZDO_JoinConfirmCB.

  • 根據我的了解是在ZDApp.c的ZDApp_ProcessNetworkJoin修改下面紅色的部份

        if (nwkStatus == ZSuccess)
        {
          //When the device has successfully rejoined then reset retryCnt
          retryCnt = 0;

          // Verify NWK key is available before sending Device_annce
          if ( ZG_SECURE_ENABLED && ( ZDApp_RestoreNwkKey( TRUE ) == false ) )
          {
            if ( ZSTACK_END_DEVICE_BUILD )
            {
              NLME_SetPollRate( zgRejoinPollRate );
            }

            // wait for auth from trust center
            ZDApp_ChangeState( DEV_END_DEVICE_UNAUTH );

            // Start the reset timer for MAX UNAUTH time
            ZDApp_ResetTimerStart( MAX_DEVICE_UNAUTH_TIMEOUT );
          }
          else
          {
            ZDApp_ChangeState( DEV_END_DEVICE );

            osal_stop_timerEx( ZDAppTaskID, ZDO_REJOIN_BACKOFF );

            // setup Power Manager Device
    #if defined ( POWER_SAVING )
            osal_pwrmgr_device( PWRMGR_BATTERY );
    #endif

            // The receiver is on, turn network layer polling off.
            if ( ZDO_Config_Node_Descriptor.CapabilityFlags & CAPINFO_RCVR_ON_IDLE )
            {
              // if Child Table Management process is not enabled
              if ( zgChildAgingEnable == FALSE )
              {
                NLME_SetPollRate( 0 );
                NLME_SetQueuedPollRate( 0 );
                NLME_SetResponseRate( 0 );
              }
            }

            if ( ZSTACK_ROUTER_BUILD )
            {
              // NOTE: first two parameters are not used, see NLMEDE.h for details
              if ( ZDO_Config_Node_Descriptor.LogicalType != NODETYPE_DEVICE )
              {
                NLME_StartRouterRequest( 0, 0, false );
              }
            }

            ZDApp_AnnounceNewAddress();

            if ( ( (ZDO_Config_Node_Descriptor.CapabilityFlags & CAPINFO_RCVR_ON_IDLE) == 0 )
                || ( (ZDO_Config_Node_Descriptor.CapabilityFlags & CAPINFO_RCVR_ON_IDLE)
                  && (zgChildAgingEnable == TRUE) ) )
            {
              if(devStartMode == MODE_REJOIN)
              {
                NLME_SetPollRate( zgRejoinPollRate );
              }
              else
              {
                NLME_SetPollRate( ZDApp_SavedPollRate );
              }
            }
          }
        }
        else
        {
          if ( devStartMode == MODE_RESUME )
          {
            if ( ++retryCnt <= MAX_RESUME_RETRY )
            {
              if ( _NIB.nwkPanId == 0xFFFF )
                devStartMode = MODE_JOIN;
              else
              {
                devStartMode = MODE_REJOIN;
                _tmpRejoinState = true;
                prevDevState = DEV_NWK_SEC_REJOIN_CURR_CHANNEL;
              }
            }
            // Do a normal join to the network after certain times of rejoin retries
            else if( AIB_apsUseInsecureJoin == true )
            {
              devStartMode = MODE_JOIN;
            }
          }
          else if(devStartMode == MODE_REJOIN)
          {
            if ( ZSTACK_END_DEVICE_BUILD )
            {
              devStartMode = MODE_REJOIN;
              _tmpRejoinState = true;
              _NIB.nwkState = NWK_INIT;

              if( prevDevState == DEV_NWK_SEC_REJOIN_CURR_CHANNEL )
              {
                runtimeChannel = MAX_CHANNELS_24GHZ;
                prevDevState = DEV_NWK_SEC_REJOIN_ALL_CHANNEL ;
              }
              else if ( prevDevState == DEV_NWK_SEC_REJOIN_ALL_CHANNEL)
              {
                // Set the flag that will ask the device to do trust center network layer rejoin.
                _NIB.nwkKeyLoaded = FALSE;
                ZDApp_ResetNwkKey(); // Clear up the old network key.
                runtimeChannel = (uint32) (1L << _NIB.nwkLogicalChannel);
                prevDevState = DEV_NWK_TC_REJOIN_CURR_CHANNEL ;
              }
              else if ( prevDevState == DEV_NWK_TC_REJOIN_CURR_CHANNEL )
              {
                runtimeChannel = MAX_CHANNELS_24GHZ;
                prevDevState= DEV_NWK_TC_REJOIN_ALL_CHANNEL ;
              }
              NLME_SetPollRate( zgRejoinPollRate );
            }
          }

          // Clear the neighbor Table and network discovery tables.
          nwkNeighborInitTable();
          NLME_NwkDiscTerm();

          // setup a retry for later...
          ZDApp_NetworkInit( (uint16)(NWK_START_DELAY
               + (osal_rand()& EXTENDED_JOINING_RANDOM_MASK)) );
        }