This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

在Z-Stack 3.0.2中协调器CC2538开启PA CC2592,终端节点距离协调器20米处就断线

Other Parts Discussed in Thread: CC2538, CC2592, CC2530

协议栈:Z-Stack3.0.2

协调器处理器:CC2538 + CC2592

终端设备处理器:CC2530

问题描述:

协调器CC2538开启PA CC2592功能(#define HAL_PA_LNA_CC2592),再用“macRadioSetTxPower(20);”设置发射功率为20dBm。

拿终端设备慢慢远离协调器,当终端设备里协调器20米左右时与协调器断开连接。抓包可以看到终端发送的“data request”请求,但是协调器无“ack”回复。

CC2538与CC2593连接的引脚是官方的连接引脚:PC2-LAN_EN、PC3-PA_EN、PD2-HGM

问题:

1、请问Z-Stack3.0.2协议栈底层有限制发射功率和接收灵敏度吗?

2、Green Power功能会对协调器的发射功率和接收灵敏度产生影响吗?

3、为什么用Z-Stack3.0.2协议栈只能传输20米的距离?

4、有关于Z-Stack3.0.2协议栈发射功率和接收灵敏度功能描述的文档吗?