Other Parts Discussed in Thread: CC2530, Z-STACK
芯片为cc2530 ,协议栈使用的是home 1.2.2a.问题如下:
1.如何设置设备多信道扫描,比如我需要设备依次扫描信道11 ,15 ,20,需要如何配置?
2.如何设置设备扫描同一个信道的次数,以及发送信标帧的间隔时间?
3.如何限制设备总的扫描时间,比如我只需要设备找网1min,如果1min之内没有找到网络,则设备休眠,如何设置?
4.如何限制设备rejoin时间?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我这边选择了多个信道,配置如下:
/* Default channel is Channel 11 - 0x0B */
// Channels are defined in the following:
// 0 : 868 MHz 0x00000001
// 1 - 10 : 915 MHz 0x000007FE
// 11 - 26 : 2.4 GHz 0x07FFF800
//
//-DMAX_CHANNELS_868MHZ 0x00000001
//-DMAX_CHANNELS_915MHZ 0x000007FE
//-DMAX_CHANNELS_24GHZ 0x07FFF800
//-DDEFAULT_CHANLIST=0x04000000 // 26 - 0x1A
//-DDEFAULT_CHANLIST=0x02000000 // 25 - 0x19
//-DDEFAULT_CHANLIST=0x01000000 // 24 - 0x18
//-DDEFAULT_CHANLIST=0x00800000 // 23 - 0x17
//-DDEFAULT_CHANLIST=0x00400000 // 22 - 0x16
//-DDEFAULT_CHANLIST=0x00200000 // 21 - 0x15
-DDEFAULT_CHANLIST=0x00100000 // 20 - 0x14
//-DDEFAULT_CHANLIST=0x00080000 // 19 - 0x13
//-DDEFAULT_CHANLIST=0x00040000 // 18 - 0x12
//-DDEFAULT_CHANLIST=0x00020000 // 17 - 0x11
//-DDEFAULT_CHANLIST=0x00010000 // 16 - 0x10
-DDEFAULT_CHANLIST=0x00008000 // 15 - 0x0F
//-DDEFAULT_CHANLIST=0x00004000 // 14 - 0x0E
//-DDEFAULT_CHANLIST=0x00002000 // 13 - 0x0D
//-DDEFAULT_CHANLIST=0x00001000 // 12 - 0x0C
-DDEFAULT_CHANLIST=0x00000800 // 11 - 0x0B
之后设备在找网的时候只会在11信道找网,不会自动切换信道,这个需要手动设置吗?如果我把DEFAULT_CHANLIST设置成0x00108800,设备找网会自动切换信道吗?