Other Parts Discussed in Thread: Z-STACK
根据下面链接来修改的,协调器2538,终端2530,都是基于3.0.2协议栈(HomeAutomation)

1.关于第24条的修改:
修改为 i = (gMAX_NWK_SEC_MATERIAL_TABLE_ENTRIES - 1); // ADD THIS LINE
请问这里的修改是不是协调器和终端里面都需要修改?
2.关于第18条的修改:
In ZDApp_ProcessNetworkJoin of ZDApp.c, remove NLME_SetPollRate( zgRejoinPollRate ); from if
(nwkStatus == ZSuccess) and place in the else statement instead. One must also set the
zgRejoinPollRate when device state is DEV_END_DEVICE_UNAUTH
2.1:这句话具体怎么修改?NLME_SetPollRate( zgRejoinPollRate )放在else的什么位置?
2.2:One must also set the
zgRejoinPollRate when device state is DEV_END_DEVICE_UNAUTH
这个具体怎么设置呢?
Optimally, also place NLME_SetPollRate( ZDApp_SavedPollRate ); inside of ZDO_JoinConfirmCB
2.3:这句话具体怎么修改?NLME_SetPollRate( ZDApp_SavedPollRate );放在ZDO_JoinConfirmCB的哪个位置?
2.4:关于第18条的修改是协调器和终端都需要修改吗?