This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于zstack 3.0.2的bug修改说明

Other Parts Discussed in Thread: Z-STACK

根据下面链接来修改的,协调器2538,终端2530,都是基于3.0.2协议栈(HomeAutomation)

[FAQ] CC2538: Z-Stack 3.0.2 Known Issues and Fixes - Zigbee & Thread forum - Zigbee & Thread - TI E2E...

e2e.ti.com
Part Number: CC2538 Other Parts Discussed in Thread: CC2531 , CC2530 , Z-STACK , , CC2592 This page contains known issues on the published Zigbee Software releases

1.关于第24条的修改:

修改为   i = (gMAX_NWK_SEC_MATERIAL_TABLE_ENTRIES - 1); // ADD THIS LINE

请问这里的修改是不是协调器和终端里面都需要修改?

2.关于第18条的修改:

In ZDApp_ProcessNetworkJoin of ZDApp.c, remove NLME_SetPollRate( zgRejoinPollRate ); from if
(nwkStatus == ZSuccess) and place in the else statement instead. One must also set the
zgRejoinPollRate when device state is DEV_END_DEVICE_UNAUTH

2.1:这句话具体怎么修改?NLME_SetPollRate( zgRejoinPollRate )放在else的什么位置?

2.2:One must also set the
zgRejoinPollRate when device state is DEV_END_DEVICE_UNAUTH

这个具体怎么设置呢?

Optimally, also place NLME_SetPollRate( ZDApp_SavedPollRate ); inside of ZDO_JoinConfirmCB

2.3:这句话具体怎么修改?NLME_SetPollRate( ZDApp_SavedPollRate );放在ZDO_JoinConfirmCB的哪个位置?

2.4:关于第18条的修改是协调器和终端都需要修改吗?

  • 只改一处就可以了,第二个也是只改一处
    其余的我看下,之后回复你
  • 1.关于第24条的修改:

    修改为 i = (gMAX_NWK_SEC_MATERIAL_TABLE_ENTRIES - 1); // ADD THIS LINE

    请问这里的修改是修改协调器还是终端还是都要修改?
  • 基本上就把所有的補釘都打上去你不用去管协调器还是终端是不是都要修改,你編譯的時候選好要协调器还是终端就行了
  • 关于第18条的修改:

    In ZDApp_ProcessNetworkJoin of ZDApp.c, remove NLME_SetPollRate( zgRejoinPollRate ); from if
    (nwkStatus == ZSuccess) and place in the else statement instead. One must also set the
    zgRejoinPollRate when device state is DEV_END_DEVICE_UNAUTH

    1. remove NLME_SetPollRate( zgRejoinPollRate ); from if
    (nwkStatus == ZSuccess) and place in the else statement instead.
    NLME_SetPollRate( zgRejoinPollRate )放在else的什么位置?

    2.One must also set the
    zgRejoinPollRate when device state is DEV_END_DEVICE_UNAUTH

    这个具体怎么设置呢?

    3.Optimally, also place NLME_SetPollRate( ZDApp_SavedPollRate ); inside of ZDO_JoinConfirmCB

    NLME_SetPollRate( ZDApp_SavedPollRate );放在ZDO_JoinConfirmCB的哪个位置?
  • 1&2

          if ( ZG_SECURE_ENABLED && ( ZDApp_RestoreNwkKey( TRUE ) == false ) )
          {
            //if ( ZSTACK_END_DEVICE_BUILD )
            //{
            //  NLME_SetPollRate( zgRejoinPollRate );
            //}
            // wait for auth from trust center
            ZDApp_ChangeState( DEV_END_DEVICE_UNAUTH );
            
            bdb_nwkAssocAttemt(TRUE);
          }
    ...
        if (nwkStatus == ZSuccess)
        {
          //When the device has successfully rejoined then reset retryCnt
          retryCnt = 0;
    
          // Verify NWK key is available before sending Device_annce
          if ( ZG_SECURE_ENABLED && ( ZDApp_RestoreNwkKey( TRUE ) == false ) )
          {
            //加在這
            if ( ZSTACK_END_DEVICE_BUILD )
            {
              NLME_SetPollRate( zgRejoinPollRate );
            }
            // wait for auth from trust center
            ZDApp_ChangeState( DEV_END_DEVICE_UNAUTH );
    
            // Start the reset timer for MAX UNAUTH time
            ZDApp_ResetTimerStart( MAX_DEVICE_UNAUTH_TIMEOUT );
          }
    

    3. ZDO_JoinConfirmCB的最後一行就可以

  • 你的协调器2538、终端2530是不同的平台,所以二者都需要修改
  • In ZDApp_ProcessNetworkJoin of ZDApp.c, remove NLME_SetPollRate( zgRejoinPollRate ); from if
    (nwkStatus == ZSuccess) and place in the else statement instead. One must also set the
    zgRejoinPollRate when device state is DEV_END_DEVICE_UNAUTH
    关于上面一句话的理解,还是不太明白,是不是下面函数的两个地方都要修改?
    下面的函数有两个地方都有if ( nwkStatus == ZSuccess )
    void ZDApp_ProcessNetworkJoin( void )
    {
    if ( (devState == DEV_NWK_JOINING) ||
    ((devState == DEV_NWK_ORPHAN) &&
    (ZDO_Config_Node_Descriptor.LogicalType == NODETYPE_ROUTER)) )
    {
    // Result of a Join attempt by this device.
    if ( nwkStatus == ZSuccess )
    {
    osal_set_event( ZDAppTaskID, ZDO_STATE_CHANGE_EVT );
    
    #if defined ( POWER_SAVING )
    osal_pwrmgr_device( PWRMGR_BATTERY );
    #endif
    
    if ( ZG_SECURE_ENABLED && ( ZDApp_RestoreNwkKey( TRUE ) == false ) )
    {
    if ( ZSTACK_END_DEVICE_BUILD )
    {
    NLME_SetPollRate( zgRejoinPollRate );//这里注释吗?
    }
    // wait for auth from trust center
    ZDApp_ChangeState( DEV_END_DEVICE_UNAUTH );
    
    bdb_nwkAssocAttemt(TRUE);
    }
    else
    {
    if ( ZSTACK_ROUTER_BUILD )
    {
    if ( devState == DEV_NWK_ORPHAN
    && ZDO_Config_Node_Descriptor.LogicalType != NODETYPE_DEVICE )
    {
    // Change NIB state to router for restore
    _NIB.nwkState = NWK_ROUTER;
    }
    }
    
    if ( devState == DEV_NWK_JOINING )
    {
    ZDApp_AnnounceNewAddress();
    if( bdbCommissioningProcedureState.bdbCommissioningState == BDB_COMMISSIONING_STATE_TL )
    {
    bdb_setNodeIsOnANetwork(TRUE);
    bdb_reportCommissioningState( BDB_COMMISSIONING_STATE_TL, TRUE );
    }
    }
    
    ZDApp_ChangeState( DEV_END_DEVICE );
    
    if ( ZSTACK_ROUTER_BUILD )
    {
    // NOTE: first two parameters are not used, see NLMEDE.h for details
    if ( ZDO_Config_Node_Descriptor.LogicalType != NODETYPE_DEVICE )
    {
    NLME_StartRouterRequest( 0, 0, false );
    }
    }
    }
    }
    else
    {
    
    bdb_nwkAssocAttemt(FALSE);
    
    NLME_SetPollRate( zgRejoinPollRate );//这里添加?
    }
    }
    else if ( devState == DEV_NWK_ORPHAN ||
    devState == DEV_NWK_SEC_REJOIN_CURR_CHANNEL ||
    devState == DEV_NWK_TC_REJOIN_CURR_CHANNEL ||
    devState == DEV_NWK_TC_REJOIN_ALL_CHANNEL ||
    devState == DEV_NWK_SEC_REJOIN_ALL_CHANNEL )
    {
    // results of an orphaning attempt by this device
    if (nwkStatus == ZSuccess)
    {
    //When the device has successfully rejoined then reset retryCnt
    retryCnt = 0;
    
    // Verify NWK key is available before sending Device_annce
    if ( ZG_SECURE_ENABLED && ( ZDApp_RestoreNwkKey( TRUE ) == false ) )
    {
    if ( ZSTACK_END_DEVICE_BUILD )
    {
    NLME_SetPollRate( zgRejoinPollRate );//这里注释?
    }
    // wait for auth from trust center
    ZDApp_ChangeState( DEV_END_DEVICE_UNAUTH );
    
    // Start the reset timer for MAX UNAUTH time
    ZDApp_ResetTimerStart( MAX_DEVICE_UNAUTH_TIMEOUT );
    }
    else
    {
    ZDApp_ChangeState( DEV_END_DEVICE );
    
    osal_stop_timerEx( ZDAppTaskID, ZDO_REJOIN_BACKOFF );
    
    // setup Power Manager Device
    #if defined ( POWER_SAVING )
    osal_pwrmgr_device( PWRMGR_BATTERY );
    #endif
    
    // The receiver is on, turn network layer polling off.
    if ( ZDO_Config_Node_Descriptor.CapabilityFlags & CAPINFO_RCVR_ON_IDLE )
    {
    // if Child Table Management process is not enabled
    if ( zgChildAgingEnable == FALSE )
    {
    NLME_SetPollRate( 0 );
    NLME_SetQueuedPollRate( 0 );
    NLME_SetResponseRate( 0 );
    }
    }
    
    if ( ZSTACK_ROUTER_BUILD )
    {
    // NOTE: first two parameters are not used, see NLMEDE.h for details
    if ( ZDO_Config_Node_Descriptor.LogicalType != NODETYPE_DEVICE )
    {
    NLME_StartRouterRequest( 0, 0, false );
    }
    }
    
    ZDApp_AnnounceNewAddress();
    }
    }
    else
    {
    if ( devStartMode == MODE_RESUME )
    {
    if ( ++retryCnt <= MAX_RESUME_RETRY )
    {
    if ( _NIB.nwkPanId == 0xFFFF )
    devStartMode = MODE_JOIN;
    else
    {
    devStartMode = MODE_REJOIN;
    _tmpRejoinState = true;
    prevDevState = DEV_NWK_SEC_REJOIN_CURR_CHANNEL;
    }
    }
    // Do a normal join to the network after certain times of rejoin retries
    else if( AIB_apsUseInsecureJoin == true )
    {
    devStartMode = MODE_JOIN;
    }
    }
    else if(devStartMode == MODE_REJOIN)
    {
    if ( ZSTACK_END_DEVICE_BUILD )
    {
    devStartMode = MODE_REJOIN;
    _tmpRejoinState = true;
    _NIB.nwkState = NWK_INIT;
    }
    }
    
    // Clear the neighbor Table and network discovery tables.
    nwkNeighborInitTable();
    NLME_NwkDiscTerm();
    
    if ( ( ( (ZDO_Config_Node_Descriptor.CapabilityFlags & CAPINFO_RCVR_ON_IDLE) == 0 )
    || ( (ZDO_Config_Node_Descriptor.CapabilityFlags & CAPINFO_RCVR_ON_IDLE)
    && (zgChildAgingEnable == TRUE) ) ) && (devStartMode == MODE_REJOIN) )
    {
    NLME_SetPollRate( zgRejoinPollRate );
    }
    }
    
    NLME_SetPollRate( zgRejoinPollRate );//这里添加?
    }
    #if defined ( ZIGBEEPRO )
    else if ( devState != DEV_HOLD )
    {
    #ifdef APP_TP2
    if(devState == DEV_END_DEVICE_UNAUTH )
    {
    return;
    }
    #endif
    
    // Assume from address conflict
    
    // Notify the network
    ZDApp_AnnounceNewAddress();
    
    // Notify apps
    osal_set_event( ZDAppTaskID, ZDO_STATE_CHANGE_EVT );
    }
    #endif
    }
    

  • poll rate 的修改只會套用到END DEVICE,我也已經指示你修改的地方了
  • 上面你是指出了,但是你改的程序跟那个说明的不一样啊?
    remove NLME_SetPollRate( zgRejoinPollRate ); from if
    (nwkStatus == ZSuccess) and place in the else statement instead. One must also set the
    zgRejoinPollRate when device state is DEV_END_DEVICE_UNAUTH
    这句话的意思是
    if (nwkStatus == ZSuccess)
    {
    NLME_SetPollRate( zgRejoinPollRate );//注释掉
    }
    else
    {
    NLME_SetPollRate( zgRejoinPollRate );//加在这里
    }
    但是你给的程序还是加在if (nwkStatus == ZSuccess)里的啊?
    if ( (devState == DEV_NWK_JOINING) ||
    ((devState == DEV_NWK_ORPHAN) &&
    (ZDO_Config_Node_Descriptor.LogicalType == NODETYPE_ROUTER)) )
    和else if ( devState == DEV_NWK_ORPHAN ||
    devState == DEV_NWK_SEC_REJOIN_CURR_CHANNEL ||
    devState == DEV_NWK_TC_REJOIN_CURR_CHANNEL ||
    devState == DEV_NWK_TC_REJOIN_ALL_CHANNEL ||
    devState == DEV_NWK_SEC_REJOIN_ALL_CHANNEL )
    这两个if里面都有if (nwkStatus == ZSuccess)语句,都要修改吗?
  • 帮忙解答下 @Kevin Qiu1 @YiKai Chen
  • https://e2echina.ti.com/question_answer/wireless_connectivity/zigbee/f/104/t/161613?tisearch=e2e-quicksearch&amp;keymatch=NLME_SetPollRate(%20zgRejoinPollRate%20)

    这是你之前回复的,我现在是基于3.0.2协议栈(HA),是不是这个bug已经更新过了?你之前发的修改方法,实在没看明白

    Proposed fix:
    In ZDApp_ProcessNetworkJoin of ZDApp.c, remove NLME_SetPollRate( zgRejoinPollRate ); from if
    (nwkStatus == ZSuccess) and place in the else statement instead. One must also set the
    zgRejoinPollRate when device state is DEV_END_DEVICE_UNAUTH

    Optimally, also place NLME_SetPollRate( ZDApp_SavedPollRate ); inside of ZDO_JoinConfirmCB.

  • 剛剛比對了一下,看起來Z-STACK 3.0.2預設已經有PATCH這個項目了,所以你不用再PATCH

  • 你好,下面函数的新增加了i = (gMAX_NWK_SEC_MATERIAL_TABLE_ENTRIES - 1); 一行以后
    NWK_FRAMECOUNTER_CHANGES_RESTORE_DELTA 要不要从默认的250 改为1000或者3000?
    如果需要改建议改为多少?
    ZDApp_RestoreNwkSecMaterial
    {
    ……
    if(nwkSecMaterialDesc.FrameCounter)
    {
    UpdateFrameCounter = TRUE;
    i = (gMAX_NWK_SEC_MATERIAL_TABLE_ENTRIES - 1); //添加此行
    }
    ……
    }
  • NWK_FRAMECOUNTER_CHANGES_RESTORE_DELTA不用更動
x 出现错误。请重试或与管理员联系。