This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-CC26X2R1: OTA_SERVER(PC軟體)自行製作的參考文件.

Part Number: LAUNCHXL-CC26X2R1

HI YK

這幾天大概喵了一下"MONITOR AND TEST API"
裡面有提到可以OTA的只有

AF_DATA_STORE這一個CMD??

看內容蠻像的啦,傳送大量DATA, 只是你在用的是
時候如果是拿來OTA,長度要為"0"??

然後想像了一下好像在PC軟體這邊也不用做很多.

它要做的工作大概就是:

1:透過UART找到OTA_SERVER

2:找到OTA_SERVER後跟OTA_SERVER要它現在到底有幾顆終端在網內.

3:把.ZIGBERR切成很小塊小塊慢慢丟到你要的那顆終端去.

4:一邊丟一邊和確認終端有ACK回來(假設)

應該這些都是己經定死的程序.因為也不可能去動ZC或ZR的OTA_SERVER專案.

只是有一個奇怪的地方,有試著拿ZR_OTA_SERVER 去和B_TOOLS連.

目前還在試那些命令可用, 但是好像會定時丟一段格式正確的DATA出來,

但B_TOOLS不知道是什麼意思??

所以想問一下OTA_SERVER是不是還需要其他參考的文件,謝謝.