打开CC2591,开启发射模式,能够正常使用;
打开CC2591,开启接收模式,无论设置成低增益还是高增益信号均无法实现放大。(使用信号源做激励,用频谱仪观察)。请问有哪位遇到过类似问题,望帮忙解答。谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我的2530+2591板子,发射功率确实比较大。但是接收灵敏度确很低。
实验条件:将USB DONGLE和2530+2591板子放在一起。2530+2591作为协调器,另外那一个节点入网后,将节点逐步远离协调器,走出20米开外,
节点就掉网。USB DONGLE探测到的节点最后数据的LQI有45。在这个距离下节点重新入网的几率比较小,这个是否说明2530+2591接收灵敏度非常低?
软件配置,默认的,硬件也是对应的:
HAL_PA_LNA_RX_HGM();
/* Raises the CCA threshold to about -70 dBm input level.
*/
CCACTRL0 = CCA_THR_HGM; //#define CCA_THR_HGM 0x06 /* 6-76=-70dBm when CC2530 operated with CC2591 in HGM */
/* Select power register value table and RSSI adjustment value table */
MAC_SetRadioRegTable(MAC_CC2591_TX_PWR_TABLE_IDX, MAC_CC2591_HGM_RSSI_ADJ_IDX);
另外请教怎么样测试2591的灵敏度?