Other Parts Discussed in Thread: CC2538
各位TI的工程师:
大家好,我最近在用CC2538的芯片跑程序,用了TI的swrc271a\cc2538_foundation_firmware_1_0_1_0\driverlib\cc2538\examples\startup_files\startup_ccs.c和cx2538xf53_ccs.cmd来建立项目,当我下载程序到CC2538一开始程序在不断运行,出现如下提示:
Cortex_M3_0: GEL Output:
Memory Map Initialization Complete
Cortex_M3_0: Can't Run Target CPU: (Error -1268 @ 0x90001) Device is locked up in Hard Fault or in NMI. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 5.1.402.0)
Cortex_M3_0: Can't Run Target CPU: (Error -1268 @ 0x90001) Device is locked up in Hard Fault or in NMI. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 5.1.402.0)
Cortex_M3_0: Can't Run Target CPU: (Error -1268 @ 0x90001) Device is locked up in Hard Fault or in NMI. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 5.1.402.0)
Cortex_M3_0: Can't Run Target CPU: (Error -1268 @ 0x90001) Device is locked up in Hard Fault or in NMI. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 5.1.402.0)
IcePick_C: GEL: Error while executing GEL_Waiting = 1: identifier not found: GEL_Waiting at GEL_Waiting=1 .
IcePick_C: GEL: Error while executing WaitForSignal(): 'WaitForSignal()' not found at WaitForSignal() .
Cortex_M3_0: AutoRun: Target not run as breakpoint could not be set: Cannot enable while the target is free running
Cortex_M3_0: Trouble Halting Target CPU: (Error -2012 @ 0x0) Requested operation cannot be done while device is running. Halt the device, and retry the operation. (Emulation package 5.1.402.0)
Cortex_M3_0: GEL Output:
Still waiting for Reset to complete
1、我查了硬件电路,reset引脚上电时电压0.8V,仿真后下载程序进去再测reset引脚变成3.2V左右,拔出仿真器又变回0.8V。这是电压没有上拉还是给MCU拉低了电压导致复位?
2、出现这个错误的原因是什么?是内存映射出错还是硬件的问题
希望能够给我点提示和帮助,万分感谢。