This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

如何提高cc2530每条指令的执行速度?希望Zigbee 大牛或IT员工能帮办解答下

Other Parts Discussed in Thread: CC2430, CC2530

我想问下,如何提高每条指令的执行速度?网上查了下,貌似可以改时钟周期,也就是提高节拍数,我在OnBoard.h 文件中找到代码如下:

// Timer clock and power-saving definitions
#define TIMER_DECR_TIME 1 // 1ms - has to be matched with TC_OCC

/* OSAL timer defines */
#define TICK_TIME 1000 // Timer per tick - in micro-sec
/*
Timer4 interrupts @ 1.0 msecs using 1/128 pre-scaler
TICK_COUNT = (CPUMHZ / 128) / 1000
*/
#define TICK_COUNT 1 // 32 Mhz Output Compare Count

/* CC2430 DEFINITIONS */

我把TIMER_DECR_TIME改为0.1, define TICK_TIME改为100 ,可每条指令的执行速度还是没提升上去,怎么回事?急需使用,希望知道的同事解答下,不胜感激。