Other Parts Discussed in Thread: CC2430, CC2530
我想问下,如何提高每条指令的执行速度?网上查了下,貌似可以改时钟周期,也就是提高节拍数,我在OnBoard.h 文件中找到代码如下:
// Timer clock and power-saving definitions
#define TIMER_DECR_TIME 1 // 1ms - has to be matched with TC_OCC
/* OSAL timer defines */
#define TICK_TIME 1000 // Timer per tick - in micro-sec
/*
Timer4 interrupts @ 1.0 msecs using 1/128 pre-scaler
TICK_COUNT = (CPUMHZ / 128) / 1000
*/
#define TICK_COUNT 1 // 32 Mhz Output Compare Count
/* CC2430 DEFINITIONS */
我把TIMER_DECR_TIME改为0.1, define TICK_TIME改为100 ,可每条指令的执行速度还是没提升上去,怎么回事?急需使用,希望知道的同事解答下,不胜感激。