This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2538 硬件设计中关于引脚问题(包括UART引脚,I2C引脚、ADC引脚等)

Other Parts Discussed in Thread: CC2538

在做CC2538时遇到如下问题,2538的硬件手册中只提供了部分引脚说明(如UART1 的,但是没有UART2的说明)。

1、 下载方式有哪些,如何实现?

2、 2线JTAG和4线JTAG区别?硬件电路?

3、 如果不使用USB功能,DVDD_USB、DGND_USB、USB_P、USB_N,这4个引脚如何处理?

4、 资料上写有,外设有2路UART,I2C,ADC,手册上没有注明(目前只知道PA0是RXD,PA1是TXD)。这些外设的引脚各是哪些?

5、 定时器的PWM输出引脚有哪些?

6、 资料上说,芯片含有上电复位电路,原理图中的nReset有何作用?

7、 将TI网站上提供的Gerber文件转化为PCB文件失败,能否直接提供PCB文件以便参考?

  • 你好,

    1, CC2538是标准的ARM芯片,看ARM的下载方式  User guide 第6章

    2,http://baike.baidu.com/link?url=alWXerhdP6t-Rg_1x63TVtns4kBijtwSNhluPcDFnYZPxKFtFcYaoG5msEAzrS17io_d7rQ362yA6B7Suvyxiq 

    3,不使用USB的话,这几个脚可以用。

    4,User guide上有说明的IOC_I2CMSSDA寄存器之类的

    5,http://e2e.ti.com/support/wireless_connectivity/f/155/t/279509.aspx 

    6,用于外部手动复位,按键复位

  • 多谢VV大神,幸亏找到你的回答了,看来CC2538的功能脚并不是固定几个脚做功能复用,而是可以通过软件指定任何GPIO脚作为功能脚的,比如UART、I2C等等功能,是吧