Other Parts Discussed in Thread: CC2530, CC2630
你好,
最近进行CC2530项目的开发,目前产品设计原型已经完成,但是射频部分的性能如通信距离还不是很理想,估计PCB设计中的阻抗没有很好匹配导致的,这里有问题想请教下:
设计中,CC2530芯片两个射频引脚RF_N和RF_P,经过一个分立元件(电感电容)的巴伦电路将平衡输出信号转换为50欧姆非平衡信号。然后通过PCB板上的50欧姆印制传输线,输送给50欧姆天线。这里射频信号经过balun转换后,50欧姆非平衡输出->50欧姆PCB传输线->50欧姆天线,这部分比较清楚,只要控制阻抗,射频功率有效传输到天线的。现在问题是:
1)射频信号从芯片的RF_N和RF_P出来经过,经过分立元件转成50欧姆的非平衡输出,这里的阻抗匹配不是很明白。RF_N/RF_P到平衡-非平衡转换电路之间的PCB走线宽度大小,对信号传输效率的影响究竟有多大?是否会导致这一级阻抗不匹配,能否通过调节平衡-非平衡转换电路中的电感或者电容进行修正,具体应该如何调节。
2)射频信号从芯片的RF_N和RF_P出来经过,如果经过一个巴伦器件2450BM15A0002将射频信号转换为非平衡输出,则RF_N/RF_P引脚和巴伦器件之间的PCB走线应该控制多少欧姆?是否通过调节线宽达到匹配?应该如何调整才能匹配?
谢谢