ZSTACK 2.5.1a的sampleapp写串口透传的时候,
1、发送数据包超过98个字节会返回afStatus_NO_ROUTE,无法发送
2、通过串口隔300ms发送数据包有规律出现丢包,返回的错误也是afStatus_NO_ROUTE
请问可能是哪里出问题呢?谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
ZSTACK 2.5.1a的sampleapp写串口透传的时候,
1、发送数据包超过98个字节会返回afStatus_NO_ROUTE,无法发送
2、通过串口隔300ms发送数据包有规律出现丢包,返回的错误也是afStatus_NO_ROUTE
请问可能是哪里出问题呢?谢谢
感谢VV的回复:
1、以下是我调用的参数: 其中str为指向mtOSALSerialData_t *cmdMsg的str=cmdMsg->msg;;
AF_DataRequest(&SampleApp_Periodic_DstAddr,&SampleApp_epDesc,
SAMPLEAPP_COM_CLUSTERID, //须自定义
len,
str,
&SampleApp_TransID,
AF_DISCV_ROUTE,
AF_DEFAULT_RADIUS) == afStatus_SUCCESS)
2、如附件的图片:
下例是我分别发送95、96、98和99个字节的串口数据的抓包情况,其中95可以抓到数据,96、98提示是包过长,但是串口接收是正常的,但是99字节,是压根没收到的,有空帮看下是什么问题,纠结很久了,非常感谢帮助。