This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2630/CC2650 ZigBee Z_Stack_Home_1.2.2例程问题

Other Parts Discussed in Thread: CC2650, CC2630, CC2530, Z-STACK

下载的Z_Stack_Home_1.2.2,里面CC2630/CC2650平台的例程只能配置为End Device吗?CC2630/CC2650现在还不能组网,必须有CC2530 Coordinator的配合才可以使用吗?

  • 参考C:\Texas Instruments\Z-Stack Home 1.2.2.42930\Documents内的Z-Stack Home Sample Application User's Guide可知

    Seven sample applications are included in the Z-Stack Home installer: SampleDoorLock,SampleDoorLockController, SampleLight, SampleSwitch, SampleHeatingCoolingUnit, SampleTemperatureSensor, SampleThermostat, and the SensorTag sample application supported
    only on the CC2650 SensorTag. Each of them supports Coordinator, Router and End Device configurations when used with CC253x platforms and in CC2630/CC2650 platforms End Device is the only configuration supported.

  • 谢谢您的解答。CC2650/CC2630将来会像CC253X一样 supports Coordinator, Router and End Device吗?

  •  我编译了下协调器,RAM和Flash都不够用。可能因为其超低功耗应用场景就是终端设备吧,现在只能用CC2530作为协调器,另外就是ZNP和ZAP外挂MCU实现协调器功能,这个1.2.2是提供工程的。

  • ZNP和ZAP外挂MCU实现协调器功能,感觉这样使CC2630/CC2650的功能打折了,不能单芯片解决的话,更倾向于选择CC253x。不清楚下一个版本协议栈会不会支持协调器,起码现在这个版本很限制CC2630/CC2650的使用范围。

  • 我大概算了下,实现协调器也并不是不可,只是留给App的硬件资源就很少了。

  • CC2650/CC2630将来会像CC253X一样 supports Coordinator, Router and End Device吗?

  • @Dalin D

    会的

  • 您好,我想在也在用CC2650作end device作一个测温的项目,想跟您请教一下CC2650作为end device,用CC2530作为coordinator怎么进行组网,有没有相关的例程可以参考?

    期待您的回复