下载的Z_Stack_Home_1.2.2,里面CC2630/CC2650平台的例程只能配置为End Device吗?CC2630/CC2650现在还不能组网,必须有CC2530 Coordinator的配合才可以使用吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
参考C:\Texas Instruments\Z-Stack Home 1.2.2.42930\Documents内的Z-Stack Home Sample Application User's Guide可知
Seven sample applications are included in the Z-Stack Home installer: SampleDoorLock,SampleDoorLockController, SampleLight, SampleSwitch, SampleHeatingCoolingUnit, SampleTemperatureSensor, SampleThermostat, and the SensorTag sample application supported
only on the CC2650 SensorTag. Each of them supports Coordinator, Router and End Device configurations when used with CC253x platforms and in CC2630/CC2650 platforms End Device is the only configuration supported.