SDK:simplelink_lowpower_f3_sdk_8_40_02_01
I am currently working on a Zigbee door lock project using the CC2340R5, where the Zigbee module acts as a node, and the gateway is provided by the customer. In the .syscfg file, I have set the poll period to 3000 ms. After successfully joining the network through the gateway, I used packet capture (sniffer) to observe that the Data Request frames were initially sent every 3 seconds. However, after some time, the device started sending Data Request frames more frequently — multiple times within 3 seconds, which causes the current consumption to increase.
In contrast, when I use my own configured CC2652 coordinator, the Data Request frames are sent evenly every 3 seconds.
I would like to know whether this issue is related to the coordinator, and how can I prove whether it's caused by the coordinator or not?
The attachments are the packages caught by me using 2652 as the coordinator and by the client's coordinator respectively