This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AMC1311: AMC1311B无论输入电压是多少,输出电压都是2.55V。

Part Number: AMC1311

AMC1311B无论输入电压是多少,输出电压都是2.55V。

输入电压VDD1为5.0V,而VDD2为3.3V。

现在遇到一种失效情况,输入无论多大电压,输出都为2.55V。这是什么原因?

原理图如下所示。