Part Number: TPA3255
Other Parts Discussed in Thread: OPA1612
2-BTL设置,做了2块板。
音量在60%以下4个通道均正常。
音量开到60%以上CD通道就保护无声,AB通道继续开大音量也正常。
需要断电重启后才能恢复C、D通道的输出。
在论坛上发现有几个同我一样的问题的帖子,但是没有看到有解决办法,能否提供支持以解决问题?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
之前做过几版(两路PVDD上只有4个1uF,没有大的电解电容),音量开到最大测试都没有问题,客户希望我们在PCB的PVDD引脚处增加了2个4700uF电容。
这一版是基于以前的电路和PCB设计,只是在PVDD引脚处增加了2个4700uF电容,因为之前完整的测试过,这个新版我们在测试的时候没有将音量调到最大,到客户处确认才发现音量不能开到最大。
我们经过测试,AB、CD通道都接音箱,音量开60%以上时,AB通道正常,CD通道保护。
AB通道接音箱,CD通道空载,音量在60%以上CLIP_OTW就会出现低电平,但是不会触发保护,AB通道会正常工作,哪怕音量开到100%也不会保护。
CD通道接音箱,AB通道空载,音量在60%以上CLIP_OTW就会出现低电平,CD通道进入保护。
将增加的2个4700uF/100V的电容拆掉,故障依旧。
OC_ADJ电阻为22K, FREQ_ADJ电阻为30K。
使用电源为金升阳LOF750-20B48,48V/750W,音箱为4Ω/300W×2。
将电压调整为52V时,故障现象没有改变。电源更换为32V/750W ,音量约开到40%位置CD通道即保护。
更换输出滤波的电感电容和EVM一致,故障依旧。
更换输入差分信号,AB和CD对换,故障依旧在CD通道,看来与信号输入无关。信号输入的10uF电容更换为无极电容,故障依旧。
看到论坛有加大BST电容的建议,尝试加大到47nF/100nF,无改善,加大到470nF后芯片无输出, FAULT和CLIP-OTW均为0.
客户在催着解决问题,5000片板子待生产,愁啊。。。。。
1、AB通道是否会在一段时间后触发以最大音量播放的保护? AB通道一直以最大音量播放不会保护。CD通道超过60%立即保护。
2、是否正在使用散热器? 有使用足够的散热器,确认散热不会成为问题。
3、此版本与上一版本之间是否有物料清单更改?布局也有变化吗? 物料清单没有更改,增加了2个4700uF电容,要连接电容脚的焊盘,PVDD供电线路布线有更改。ABCD4个通道输出走线加长了,4个输出电感往下挪了35mm,PCB加长了35mm ,其他没有变动.
4、IC的测试是否都来自同一批次? IC芯片是同一批次,同一卷料。
另外我做过一些改变试图解决问题:
1、使用8Ω的扬声器,音量开到最大无问题。
2、运放单端转差分的信号输入脚(OPA1612的3脚)并联一个10K电阻到地(原先是100K),可以开到最大了,不会保护,但是输出功率变小了,这不是解决问题的办法。
3、INPUT_A、B、C、D、各串联100Ω电阻、100pF到地,然后输入芯片,音量能开到80%,超过80%AB 通道无问题。C、D通道依然会保护。
4、我现在OPA1612的3脚并联了一个30K电阻到地(原先是100K),NPUT_A、B、C、D、各串联100Ω电阻、100pF到地,然后输入芯片,音量开到最大不会保护。输入1KHz 正弦波,4Ω电阻做负载,测得最大输出功率为212W,这和315W差距太大了。
是否还有其他的办法能够做到最大输出功率达到280W(客户的最低要求)不会保护?
感谢您的回复!
关于您提出的问提,我一一进行了验证:
购买了新的样品进行验证,换到之前的板上不会保护,新的板才会保护。
关于之前播放最大音量时没有出现问题的测试的几个问题:
1、是否使用了相同的扬声器?
和之前测试是相同的扬声器,并且BTL两个输出使用的是同样的扬声器。
2、音频输入是否与当前测试相同?
音源输入是同样的信号,或者是同一个音源。
电流测试:
3、清除故障是否会解决问题,还是会一直锁定?
清除故障不会解决问题,需要断电才能恢复。
4、这种情况是发生在多个板上还是只发生在一个板上?
现在贴了10片板,这种情况发生在所有的板上,不是个例。
5、这种行为在没有连接负载的情况下也会发生吗?
空载的情况下不会发生。
Can you also provide the layout/schematic files of the previous revison?
This version is modified from the previous files, and the original previous version files were not backed up or retained。Two 4700μF capacitors have been added, the output inductor has been moved down by 35mm, and the overall PCB length has been increased by 35mm, with no other changes.
Since the previous board had no issues, I believe there is a problem with the PCB design. I have revised the PCB once again and modified the sections I identified as problematic. Once the new PCB sample arrives, I will proceed with validation and continue to provide updates afterward. Thank you!