Part Number: OPA354
您好,我在测试OPA354的指标时碰到了一些问题,数据手册中定义了-3dB带宽以及-0.1dB平坦度的指标,都是在G=1或者G=2的闭环增益下测试的。但我在测试中发现在G=1或G=2的增益下,随着输入信号频率增加,输出信号的幅值反而呈现出增加的趋势,在超过某一频率后才开始下降。这和常规意义上的运放的增益-频率曲线趋势似乎不太吻合,想知道这个原因是什么

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: OPA354
您好,我在测试OPA354的指标时碰到了一些问题,数据手册中定义了-3dB带宽以及-0.1dB平坦度的指标,都是在G=1或者G=2的闭环增益下测试的。但我在测试中发现在G=1或G=2的增益下,随着输入信号频率增加,输出信号的幅值反而呈现出增加的趋势,在超过某一频率后才开始下降。这和常规意义上的运放的增益-频率曲线趋势似乎不太吻合,想知道这个原因是什么

您好
是的,负载电容会影响带宽。请参考典型图13-15。如图14所述,需使用隔离电阻以实现0.1dB平坦度。
GBW适用于高增益(G ≥ 10)场景,而250MHz的单位增益带宽(UGB)是指OPAx354开环增益降至0dB或1V/V时的频率。