This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

使用LM324搭建仪表放大器,测量电压偏差大的问题

Other Parts Discussed in Thread: LM324

电路如图所示,目的是测量RL在不同电压(1V~6V)下的电流,VIN为直流0~3V,,R4为电流采样电阻,电阻的压差经过3个LM324搭建的仪表放大器放大55倍,送给ADC。目前的问题是经过测量,vout的值明显偏大,尤其是电流越大(采样电阻的压差越大),VOUT偏差也越大,下面是使用万用表测量的各个节点的电压(单位mv,下表中输入电压为RL上的电压),及放大倍数的计算。可以看到,电流越大,放大倍数也越大,VOUT的测量值也越大,为什么呢?失调电压也进行了补偿(将采样电阻短路,测量VOUT的值),但补偿后的值依然偏大。

  • 亲;你的LM324采购自何家?

  • 是TI的,芯片上有ti的mark

  • 仪表运放的电阻匹配要求非常精密,否则,每个输入端的增益会有差异,直接影响共模抑制。比如当增益等于 1 时,所有电阻值必须相等,在这些电阻器中只要有一只电阻值有0.1%失配,CMRR就会下降很多,所以自己搭建仪表运放时需要注意这点,这也是仪表运放价格比较高的原因之一吧。

  • 0.1%的失配会使CMRR降到66db,那1%的失配是否CMRR就只有46DB,也就是只有3%的误差,6V的共模也只有18mV的误差,并且第一级放大共模电压不会被放大,所以不应该有这么大啊。目前怀疑失调电压,但失调电压应该是可以校准掉的么?将RL断开,测空载的值,然后测试值减去空载值,失调应该校掉了吧。就是不知道失调电压是否会随着哪些值变化

x 出现错误。请重试或与管理员联系。