This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
电路如图所示,目的是测量RL在不同电压(1V~6V)下的电流,VIN为直流0~3V,,R4为电流采样电阻,电阻的压差经过3个LM324搭建的仪表放大器放大55倍,送给ADC。目前的问题是经过测量,vout的值明显偏大,尤其是电流越大(采样电阻的压差越大),VOUT偏差也越大,下面是使用万用表测量的各个节点的电压(单位mv,下表中输入电压为RL上的电压),及放大倍数的计算。可以看到,电流越大,放大倍数也越大,VOUT的测量值也越大,为什么呢?失调电压也进行了补偿(将采样电阻短路,测量VOUT的值),但补偿后的值依然偏大。
仪表运放的电阻匹配要求非常精密,否则,每个输入端的增益会有差异,直接影响共模抑制。比如当增益等于 1 时,所有电阻值必须相等,在这些电阻器中只要有一只电阻值有0.1%失配,CMRR就会下降很多,所以自己搭建仪表运放时需要注意这点,这也是仪表运放价格比较高的原因之一吧。