This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
这是一个DC自动光圈的电路图,drv+/- 和cont+/-分别接了一个线圈,这两个线圈相互抵抗,控制光圈维持在某个大小,drv是驱动线圈,count是阻尼线圈,通过pwm的占空比,就能调整光圈的开合,目前3.3v控制不了(drv最大能到1.8v),需要调到4V才能控制(drv最大到2.5v),实际测试光圈也是需要2.5v左右才能动作。
目前的疑问是这个电路如何修改,才能在3.3v电源下,让drv输出达到2.5v?
不通电时,测量drv线圈阻值192,cont线圈1.16K。
已经问过几个人,根据建议做了如下试验:
PWM降低占空比,增大R1到2M,R12增加到2K,R7降低到22K,还是没有效果。
请大牛帮忙指点一下。
谢谢您的建议,我试过了没有效果,我又换成了10K,分压已经接近到了3.3v,但是drv那里的电压还是只有1.8v。
我这个电路不会有问题吧,这是我从海思官方开发板上参考的电路,它的放大器原来用的是sgm8052,我换成了lmc6482,但器件是pintopin的,而且性能基本一致。
到目前为止已经做了无数个试验了,drv的输出就是提不上去。
您好,
您的信号频率是多少?LMC6482的GBW和SR参数与SGM8052还是相差很多的,你要输出几伏的电压,就要计算下压摆率SR是否满足要求:SR=2πf×Vpp