This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

lmc6482 电路输出不正常

Other Parts Discussed in Thread: LMC6482

这是一个DC自动光圈的电路图,drv+/- 和cont+/-分别接了一个线圈,这两个线圈相互抵抗,控制光圈维持在某个大小,drv是驱动线圈,count是阻尼线圈,通过pwm的占空比,就能调整光圈的开合,目前3.3v控制不了(drv最大能到1.8v),需要调到4V才能控制(drv最大到2.5v),实际测试光圈也是需要2.5v左右才能动作。
目前的疑问是这个电路如何修改,才能在3.3v电源下,让drv输出达到2.5v?

不通电时,测量drv线圈阻值192,cont线圈1.16K。

已经问过几个人,根据建议做了如下试验:

PWM降低占空比,增大R1到2M,R12增加到2K,R7降低到22K,还是没有效果。

请大牛帮忙指点一下。

x 出现错误。请重试或与管理员联系。