在实验中,我想做一个一个低噪声、高速的运放做一个衰减50倍的衰减器,使用的运放是OPA365,是一款50MHz、零交叉、低失真、高CMRR、RRI/O、单电源运放。原理图如下,输入信号1V vpp,衰减46.3倍。直流偏置在2.5V左右。可是输出却出现了很多的毛刺噪声。而在同样的参数下,我使用通用运放LM358得到的效果却比这个好很多,这是什么原因造成的,难道是电阻用得太大吗?芯片的电源加了大小电容滤波,同时输入输出均使用SMA接头和同轴屏蔽传输线。
黄色波形是输出信号,红色是输入信号。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
抱歉我没有找到对于CMOS运放,其输入电阻以及负反馈电阻的取值要求,CMOS运放与其他运放的区别仅找到下面文档中8.CMOS 和 JFET 放大器的输入偏置电流的区别:
对于高速运放的信号完整性基础,下面文档第7部分有写: