This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您的意思是说+15V电源和7.5V电源都是由电源仪器产生?还是说7.5V电源由电路板上的电路产生?
THS3491的1脚需要连接GND,Thermal pad 也需要连接GND,请确认这两点的接法?
在数据手册的Pin Functions表格内有说明,如下截图,
看您电路连接与下面datasheet截图完全相同,因此所使用的电路图应该是没问题的,所以请连接1脚和Thermal pad 至GND后,看是否恢复正常?
我输入为10Khz的0-1V的方波信号,同向输入引脚3波形为3.75V-4.25V的方波如下图
您实际输入的是±0.25V的方波信号是吗?没有直流成分?
THS3491有输入和输出范围限制:
输入headroom最大值是4.3V@RLOAD = 100 Ω 等表头前提条件,意思是在单电源15V供电时,0~4.3V和 (15-4.3)V~15V,即10.7V ~15V 这两个电压区间的输入信号不在THS3491的输入范围内。
建议将输入信号的DC电压设置在VS/2=7.5V处,即输入7.5V±0.25V的方波信号,看输出是否正常的?
您测试了几块板子是这种情况?如果两输入端电压相差1V,可能芯片已经损坏,因为THS3491 Differential input voltage的绝对最大额定值是±0.5V,1V已经超出了这个范围,如下datasheet截图所示: