Part Number: THS3491

按照数据手册上的连接,我利用了两个电源进行供电,一个电源供电VS=15V,另一个电源则供电VS/2=7.5V,输入利用信号发生器发出100Khz的0-1V的方波,结果当两个电源同时供电时提供VS/2=7.5V的电源显示被拉高到13.82V

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我输入为10Khz的0-1V的方波信号,同向输入引脚3波形为3.75V-4.25V的方波如下图
您实际输入的是±0.25V的方波信号是吗?没有直流成分?
THS3491有输入和输出范围限制:

输入headroom最大值是4.3V@RLOAD = 100 Ω 等表头前提条件,意思是在单电源15V供电时,0~4.3V和 (15-4.3)V~15V,即10.7V ~15V 这两个电压区间的输入信号不在THS3491的输入范围内。
建议将输入信号的DC电压设置在VS/2=7.5V处,即输入7.5V±0.25V的方波信号,看输出是否正常的?