This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

THS3491: 按照数据手册上典型的单端供电测试出现异常

Part Number: THS3491

按照数据手册上的连接,我利用了两个电源进行供电,一个电源供电VS=15V,另一个电源则供电VS/2=7.5V,输入利用信号发生器发出100Khz的0-1V的方波,结果当两个电源同时供电时提供VS/2=7.5V的电源显示被拉高到13.82V

  • 您好,

    7.5V的电压您是怎样产生的?我想可能与7.5V电压产生的电路有关,您可以附上电路图加以说明吗?

  • 图1

    图2

    整个电路的连接图如图一所示,图二为板子上的供电方法,右侧为整块板子,上方电源正电极通过电源线接板子VS焊盘负极接板子AGND焊盘提供VS=15V的电源供电。下方电源通过电源线正极连接板子VS/2焊盘,负极连接AGND焊盘提供VS/2=7.5V的供电。上述电源型号为原始问题中第二张图中的电源。

  • 您的意思是说+15V电源和7.5V电源都是由电源仪器产生?还是说7.5V电源由电路板上的电路产生?

    THS3491的1脚需要连接GND,Thermal pad 也需要连接GND,请确认这两点的接法?

  • +15V和+7.5V都是通过电源仪器产生,1脚和thermalpad未接地因为没在数据手册上看到相关信息,我去试一下谢谢

  • 在数据手册的Pin Functions表格内有说明,如下截图,

    看您电路连接与下面datasheet截图完全相同,因此所使用的电路图应该是没问题的,所以请连接1脚和Thermal pad 至GND后,看是否恢复正常?

  • 1脚和thermalpad连接至GND后解决了电源被拉高的情况,但是输出有点不大对劲,请问一下这个电路里正常的输出和输入的理论关系式是怎么样的

  • 输出应该是VOUT=(1+RF/RG)*VIN+7.5V,即5VIN+7.5V

    您输入信号是什么,输出是什么?

  • 我输入为10Khz的0-1V的方波信号,同向输入引脚3波形为3.75V-4.25V的方波如下图

    反向输入端引脚2的波形如下图

    输出波形如下图

    按照您说的公式那应该反向输入引脚2上的波形是不是要和同向输入端引脚波形基本一致为7.5V-(7.5+1)V的方波,可是按照电路连接同向输入端3号引脚的信号为[(VS/2)/2+信号发生器设置信号/2}

  • 我输入为10Khz的0-1V的方波信号,同向输入引脚3波形为3.75V-4.25V的方波如下图

    您实际输入的是±0.25V的方波信号是吗?没有直流成分?

    THS3491有输入和输出范围限制:

    输入headroom最大值是4.3V@RLOAD = 100 Ω 等表头前提条件,意思是在单电源15V供电时,0~4.3V和 (15-4.3)V~15V,即10.7V ~15V 这两个电压区间的输入信号不在THS3491的输入范围内。

    建议将输入信号的DC电压设置在VS/2=7.5V处,即输入7.5V±0.25V的方波信号,看输出是否正常的?

  • 按照您说的我调试电路后得到了正常的输出,但是我发现反向输入端的信号电压要比同向输入端的信号电压低个1V左右要使得反向输入端的电压再7.5V上跳动则输入信号的偏置电压要到9.5V,而且当输入信号频率超过100Khz后放大器信号就失真了与双端供电的带宽差之甚远,请问一下这种情况是否正常

  • 您测试了几块板子是这种情况?如果两输入端电压相差1V,可能芯片已经损坏,因为THS3491 Differential input voltage的绝对最大额定值是±0.5V,1V已经超出了这个范围,如下datasheet截图所示: