Part Number: USB2ANY
Other Parts Discussed in Thread: ALP,
您好!按照链接我将固件升级,并且显示硬件连接成功
但是并没有显示954且也没有Margin Analysis界面,可能是什么原因呢,谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,当954EVM板子和PC接上后,在PC的设备管理器中能识别到吗?
我看您截图附上,ALP的版本没问题,USB2ANY这里也能正确识别。 在information这里,往下拉看到scan Connected devices。 点击这里,如果连接好的话会出现已连接的设备。

您好,按照下面这个步骤试试:
1) Click on USB2ANY/Aardvark Setup, a new window will open.
2) Chose the existing device, in the left hand side box, and click Remove.
3) Under “Select a Daughter Board" search for the required device profile, in this case DS90UB954, and click “Add” and then “Ok”.
另外,参考下UB924 的EVMuser's guide的ALP的trouble shooting的1.12.1部分ALP Loads the Incorrect Profile的步骤: